STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

SPI Slave RX data shifted

Posted on November 21, 2017 at 17:02I'm having an issue with the LL SPI driver on the STM32L4 configured as SPI slave. My Tx buffer contains {01, 02, 03, 04, 05, 06, 07... }. When I read 7 bytes repeatedly from the slave using the Aardvark SPI maste...

Konami by Senior II
  • 1383 Views
  • 3 replies
  • 0 kudos

configuring cubemx with F429ZI and ethernet

Posted on November 21, 2017 at 20:10I am trying out ethernet with UDP. However, when I generate the files through cube mx, I am unable to get it working like they do in UM1713. I tried to compile a project, but it does not like 'ethernetif_input(&gn...

HAL_DSI_Read in High Speed mode

Posted on November 21, 2017 at 13:12I try to read data, using the HAL_DSI_Read function - in the Low Power mode I read data successfully, but when switching in the High Speed mode it is impossible to read data. Result of reading - an error on a time...

mak1308 by Associate III
  • 2339 Views
  • 3 replies
  • 0 kudos

STM32F030xC Boot Loader Options

Posted on November 21, 2017 at 15:04Does the STM32F030xC support interfacing the boot loader over I2C?  The datasheet does not list this as an option but it is listed in AN2606 over port I2C1.  Which of these are correct?

mvonahnen by Associate III
  • 1253 Views
  • 1 replies
  • 0 kudos

CubeMX Issues and Suggestions

Posted on November 21, 2017 at 15:51I am really enjoying this application to get things started, but have found a few issues as follows:Issues:>> When you configure I2C and generate the code the i2c.h files includes an extern reference to the I2C_Ha...

STMFlashLoader and STM32f767BIT

Posted on November 21, 2017 at 10:29Hallo everyone,i want to programm a STM32F767BIT controller with STMFlashLoader Demo.But there is no suitable map file. Is there a newer Version of the STMFlashLoader Demo? I use Version 2.8.0. Or has someone a wo...

mfrank9 by Associate III
  • 1563 Views
  • 3 replies
  • 0 kudos

Resolved! Slow LTDC + DSIHOST Augmented Command Mode

Posted on December 19, 2016 at 19:16We are using a STM32F769 to drive a 400x400 DSI display. What could we do to about double the current writing speed or to identify what is the bottleneck? LTDC is set up for sending data from SRAM1 for DSIHOST tha...

pertti by Associate II
  • 1971 Views
  • 3 replies
  • 0 kudos

Resolved! STM32L0 TSC Analog Switch

Posted on November 17, 2017 at 17:36Hello everyone,I was researching about the TSC (Touch Sensing Controller) of my Board Nucleo L053R8 and I found that there it has  something called 'the analog switch'.The TSC is composed of several groups. Each g...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.