2017-11-22 1:23 AM
Hi
I am late in y project and need some help with a HTTP server.
This is what I need:
a webserver for FW download which also gives me the opportunity to change IP Address and Netmask, ideal on a nucleo stmf429zi board, but any other would do as well.
One of the ST example projects should be taken as starting point, like this one:
STM32Cube_FW_F4_V1.16.0\Projects\STM324xG_EVAL\Applications\LwIP\LwIP_IAP
A teamviewer session should be
Deliverables:
- firmware project : WEbserver IAP to upload FW , set netmask, IP address , IPV4
- Git repository with 2 commits: example code of ST + all changes
- an application FW which just blinks some leds
- 1 hour team viewer session demo about what needed to be changed and why.
Any one interested? send me a PM
Thx
#stm32-iap2017-11-22 1:44 AM
I am already fully occupied with my own job and projects ...
Just want to paraphrase Frederick P. Brooks from his book 'The Mythical Man-Month':
'Adding more developers to a delayed project will delay it even further.'
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.