STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

How to change relative to absolute USB mouse for STM32?

Hello,I am making a project for myself on the STM32F405 control board KVM.This board receives data to the HOST from the mouse (this part works). Next, the MCU generates absolute coordinates. These coordinates (absolute) must be transmitted via USB to...

ok_pp by Associate III
  • 2712 Views
  • 5 replies
  • 0 kudos

Selecting a Ferrite Bead for the STM32L011

The documentation mentions placing a ferrite bead between incoming voltage and the chip's VDDA line.  Having limited knowledge of ferrite beads I'm confused as to which bead would work best.  If the DC bias current should be about 20% of the bead's r...

Resolved! faied do uart send with uart5 with stm32h7b0zb

I use cubemx generate a project with uart5. It's ok.But when I move some init codes of uart5 to function ``void SystemInit (void)`` tail as below```MPU_Config();HAL_Init();SystemClock_Config();PeriphCommonClock_Config();MX_UART5_Init();dbg_console_tx...

shengyang_0-1740353545384.png

Resolved! CAN BUS Tx not working in Normal mode

Hello !Hope you're all doing well.I have a little problem here, my CAN BUS Tx is not working on "Normal Mode"I have a bus with several nodes communicating between them without any problem, so the bus itself is not the problemIn "Loopback mode" it wor...

Touftoufe by Associate II
  • 4514 Views
  • 4 replies
  • 0 kudos

STM32F767VGT6 IO 5V TOLERANT

Quick Question.... The Docs say the STM32F767VGT6  has 166 5 V tolerant I/O's I need to put 5V pullups on some of my OUTPUT I/O  !Is the tolerance just for INPUTING ?orWill the Low transistion with a 5V pullup   say   1K   be ok !  

CTerr.1 by Associate II
  • 1150 Views
  • 2 replies
  • 1 kudos

Stm32 stopped working after soldering components

 Hi, i hope you're having a great daySo i'm working on a project involving a stm32f4 and multiple other components (an ADC and a amplifier).The stm32 is connected to the ADC via I2S and to the amplifier via I2S and also I2C.I first soldered the stm32...

kubb3 by Associate
  • 1715 Views
  • 2 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.