STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F446 USB host connection issues

Hi,I am using a STM32F446 as a USB high speed host. my device is connected to a USB3300 chip to control the micro usb port, which is then connected to a camera. My code works ~90% of the time, however sometimes the connection to the camera can be unr...

JoshDarklyLabs_0-1741049534177.png

Double ECC Error inject for STM32L5/U5

Hello Community,Is there a way to inject double Flash ECC Error in Stm32L5/U5 like it is possible in case of H7 where we can simply write some different set of words at a given address without erasing? Thanks in advance,Abhi

Resolved! GPIO & EXTI: switching between input & output

Heyho,I'm currently using a GPIO on a STM32L031 for a custom 1-wire interface, which means it's switching all the time between input and output mode (open drain).So far I have learned that the EXTI interrupt only works with GPIOs in input mode.My que...

LCE by Principal II
  • 2999 Views
  • 5 replies
  • 1 kudos

ADC1 and ADC4 readings at the same time

Hello,  I have been trying for some days to read the values incoming form both ADCs, ADC1 & ADC4, from the NUCLEO U545-REQ. The overall idea is to trigger both ADCs at the same time in output compare mode but if i try to trigger both of them at the s...

Marc3 by Associate III
  • 2595 Views
  • 5 replies
  • 0 kudos

Resolved! STM32U545RE-Q: not getting ADC1 conversion data via GPDMA

Hello everyone,  I'm currently trying to set up the two ADCs (ADC1, ADC4) on my NUCLEO-U545RE-Q for multi-channel continuous conversion via GPDMA (I've previously used an L4+, but intend to change to the U5 family for the final product and am using t...

cjb89 by Associate II
  • 7621 Views
  • 6 replies
  • 0 kudos

Resolved! STM32C092 and CAN FD transceiver selection

Greetings Everybody, I am trying my hands with CAN FD. I have selected STM32C092RC for the same application as it has can fd port. I was wondering if MCP2561/62 can fd transiver ic works with this controller. Please advice. I was also looking for sch...

Resolved! ARM CMSIS DSP for CubeMX and Keil

Hi everyone;I have select;In cube mx ->middleware and software packs -> CMSIS -> CMSIS Coremiddleware and software packs -> CMSIS - DSP middleware and software packs -> X Cube Algobuild -> DSP LibraryLater, I have select from software packs -> select...

CKILI.2 by Associate II
  • 1648 Views
  • 2 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.