2025-02-27 11:03 PM - last edited on 2025-02-28 12:02 AM by Andrew Neil
I'm working on a solution using STM32H753 MCU. HRTIM1 TIMA needs to generate short periodic 100 ns pulses periodically and drive MDMA channels. This already works fine.
In addition to above, I need to drive GPIO F8 low for a short 500 ns time window then set it again. F8 must go low synchronized to the HRTIM1 TIMA CH1 being set with max latency of 200 ns.
From AF mappings only timers TIM13 and TIM16 allows me to do this, so I moved on with TIM13.
Using SW IRQs (SET1 on HRTIM triggering ISR which starts TIM13) works fine but has too high latency (cannot get it below 2.2us running MCU at 480MHz and TIM13 at 120MHz) so gave up on that path.
I'm looking for a HW configuration solution. I have been perusing the reference manual and datasheet documentation but do not see a clear way to map this correctly. I believe I will need some sort of slave mode configuration for TIM13/TIM16 and route some OC/SETx1 event from HRTIM1 TIMA to generate a start trigger on the TIM13/TIM16 timers, but per the reference manual and datasheet it does not look like this is possible.
Out of curiosity I tried a quick CoPilot search which tells me some contrasting information. I tried it without success. It suggests:
HRTIM1->sCommonRegs.OENR |= HRTIM_OENR_TA1OEN;
TIM13->SMCR |= TIM_SMCR_TS_2 | TIM_SMCR_TS_0; // Select HRTIM TIMA event as trigger TIM13->SMCR |= TIM_SMCR_SMS_2; // Set TIM13 to trigger mode
but TIM13 is never started, so I don't think it's useful (can't find any information on SMCR availability for TIM13/TIM16 in reference manual nor in datasheet).
Please advise - this is a critical problem which I will need to address somehow. Preference is not to make a costly HW change as product is ready for pre-production.
Thank you.
2025-03-02 5:31 AM
Bad luck. TIM13 /16 don't have external trigger inputs. Use another GPIO or hardware solution.
2025-03-03 10:38 AM - edited 2025-03-03 10:48 AM
From datasheets/reference manual I would agree with @MasterT. Only problem is I've been told HW change must be prevented if possible.
As a last SW effort, I found an option to initiate a MDMA transfer triggered by an already triggered DMA on HRTIM SET1.
Configuring the MDMA transfer to point to HRTIM13 registers (all memory mapped) as destination and predefining a constant configuration enabling the TIM13 as immutable source this seems do almost do the job.
Some unexpected results which may be bugs, but this solution appears to be a way forward. Latency remains too long (~500ns for a full TIM13 configuration) but may be tweaked with the parameters sent.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.