2025-03-03 3:37 PM
Hi there,
We are working on a project in university. The objective of the project is to wirelessly transmit live camera feed to a LCD MIPI-4 Lane 50 pin screen using a digital camera module. We plan on using two microcontrollers, one for the camera which is remotely placed and one for the LCD screen that is with the user. We are wondering whether the STM32 boards we are looking to acquire are applicable for our intended applications or if any adjustments should be made.
Choice for camera microcontroller:
Choice for display microcontroller:
We are also unsure how to wirelessly transmit the feed (up to 2 miles), please suggest solutions for STM32 Microcontrollers as well.
Thank you,
Chris
2025-03-03 4:29 PM
Perhaps you should look at what resolutions and protocols UAV video solutions are using and the kinds of bandwidth and power involved
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.