STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32H7xx Example-programs

Posted on January 28, 2018 at 16:09I am using the STM32H743 together with uVision 5.Are there any example-programs available not using RTOS2 and CubeMX ?What I am missing are simple demo-programs like Blinky ( without RTX ) and a demo-programusing t...

stpmc-1 module spi driver

Posted on January 28, 2018 at 13:40I am using stm32f429igtx controller. I am trying to interface stpmc-1 energy calculator module with the controller. stpmc-1 module uses some kind of SPI protocol. I need to know whether st provided any driver file ...

Resolved! why interrup occerd when TIM1 is not ENABLE??

Posted on January 25, 2018 at 10:19hi guys.i wrote a code with IAR , and when is run the code in stm32f103ret , cpu go to  the interrupt s routin.i dont know why??!!i want to have 1msecond delay for each timer priode , but i cant do that. when the c...

STM32F7 FMC controller configuration

Posted on January 27, 2018 at 12:33Hello .,I am working on STMF7 MCU , In that I need to access external Parallel bus interfaced device. I have attached Read/write cycles of the device, Can any one suggest me which mode should I configure to access ...

I cannot get I2C work on stm32l476

Posted on January 19, 2018 at 21:59Hi All,First post on here and a newbie with the STM32 family of devices (I come from a PIC background - sorry about that)I have just received my first STM32 board design back from the sub contractors and am having ...

how to use ''printf''?

Posted on February 09, 2017 at 14:47I'm using examples of project  'UART_Printf'. But I can't use printf. I set uart1. and I checked that uart1 tx/rx works. I added below code to my source. &sharpinclude 'stdio.h'&sharpifdef __GNUC__/* With GCC/RAIS...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.