2018-01-28 7:09 AM
I am using the STM32H743 together with uVision 5.
Are there any example-programs available not using RTOS2 and CubeMX ?
What I am missing are simple demo-programs like Blinky ( without RTX ) and a demo-program
using the LCD ( without a GUI, yust a simple output of text would be fine ).
I have available a project, the only purpose shall be to switch an LED on,
it compiles, links and flashes without error, but nothing else happens...
Probably an initialisation-problem but I need a working example to get on the right path.
Solved! Go to Solution.
2018-01-28 8:16 AM
Outputting text isn't exactly simple, you have to paint the bitmaps
HAL examples are under the Cube Repository trees
\STM32Cube_FW_H7_V1.1.0\Projects\STM32H743I_EVAL\Examples\GPIO\GPIO_EXTI\Src\main.c
\STM32Cube_FW_H7_V1.1.0\Projects\STM32H743I_EVAL\Examples\UART\UART_Printf
2018-01-28 8:16 AM
Outputting text isn't exactly simple, you have to paint the bitmaps
HAL examples are under the Cube Repository trees
\STM32Cube_FW_H7_V1.1.0\Projects\STM32H743I_EVAL\Examples\GPIO\GPIO_EXTI\Src\main.c
\STM32Cube_FW_H7_V1.1.0\Projects\STM32H743I_EVAL\Examples\UART\UART_Printf
2018-01-28 9:21 AM
Custom or ST board?
In case of Nucleo or Eval, which LED did you try turn on?
2018-01-28 12:51 PM
The availability of an LCD suggests the STM32H743I-EVAL, and ST doesn't provide examples for third party boards.
2018-01-29 12:23 AM
There are already excellent examples available inside the STM32Cube-firmware-package,
Uefull as well for Keils MDK-toolchain.
I only haven't expected to find them there at first.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.