STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

TensorFlow serving vs TensorFlow service

Posted on February 13, 2018 at 07:05I have a question regarding the difference between TensorFlow Serving versus TensorFlow service. (Sorry that I'm not familiar with this at all.)I found TensorFlow serving's definition, which is 'TensorFlow Serving...

Error while debugging STM32F051R4T6TR

Posted on February 13, 2018 at 07:24We have designed a new product with STM32F051R4T6TR ic.We are using JLINK to debugg the STM controller.We using IDE :Keil version 5.After Compiling we got the following error shown below: JLink info:------------DL...

Amal Babu by Associate III
  • 1423 Views
  • 0 replies
  • 0 kudos

STEVAL-3DP001 3D Printer Board Cann't Connect PC

Posted on February 13, 2018 at 04:43Board: STEVAL-3DP001 3D Printer Board;ISSUE:  Use a GUI with virtul com port cann't connect the board;via serial port is possible with ST-LINK on the 3D printer board,the ST-LINK driver installed,Virtul com port r...

Xh Zhang by Associate
  • 593 Views
  • 0 replies
  • 0 kudos

Custom Bootloader fails to Launch App - HardFault_Handler

Posted on February 12, 2018 at 23:19I have built an STM32F303ZET6 project using the AC6 IDE and FreeRTOS.  The base application (located at 0x08000000) incorporates a mechanism for loading a new firmware image above the base application (at 0x080300...

CAN Communication with MAT-TARGET

Posted on February 08, 2018 at 20:41I am trying to run a basic example using CAN with the STM32F767ZI evaluation board using the next blocks in Simulink:But when I compile the code I get the next errors:Where should be all defined? I can't find any ...

0690X00000609bGQAQ.png 0690X00000609YbQAI.png

Resolved! Timer DMA requests through DMA1 clarification

Posted on January 24, 2018 at 10:32 Hey everyone, I need some clarification on this, as it will help my program run smoother. I want to run 2 DMA's simultaneously. One which will send data out using the SDMMC1, which is linked to DMA2. Then I'd...

0690X00000604I3QAI.jpg 0690X00000604IIQAY.jpg
con3 by Senior
  • 5839 Views
  • 17 replies
  • 0 kudos

LIS3DH library

Posted on February 12, 2018 at 11:18Hello everyone,Can someone help me with LIS3DH accelerometer library.Thank you.

Problem with STM32F37 USART1 Clock Mux on PCLK2

Posted on February 12, 2018 at 17:39Hello together,I'm working with an STM32F37 MCU and have somme issues with the USART1 Clock Mux.I enabled the Receiver Timeout Interrupt to detect the end of a Modbus message. With the HSI clock the interrupt occu...

0690X00000609WiQAI.png
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.