2018-02-12 2:18 AM
Hello everyone,
Can someone help me with LIS3DH accelerometer library.
Thank you.
2018-02-12 2:28 AM
I use the LIS33DE but this one seems to work the same way:
-set right bits here: CTRL_REG1 (20h) - mode, enable x, y, z
-then you can read the STATUS_REG (27h) register and see if the ZYXDA bit is set
-then read the particular OUTxxxx register
I assumed that you can handle the I2C/SPI bus correctly. I use SPI.
Details:
2018-02-12 7:03 AM
Here is the library I use:
https://github.com/s54mtb/LEDS/blob/master/Src/lis3dh_driver.c
2018-02-12 9:18 AM
,
,
I use simplified code:
♯ define LIS35_WRITE 0
,
♯ define LIS35_READ , , ,0x80,
♯ define LIS35_ADDR_NO_INC 0,
♯ define LIS35_ADDR_INC 0x40♯ define LIS35_REG_OUTX , , ,0x29
,
♯ define LIS35_REG_OUTY , , ,0x2B,
♯ define LIS35_REG_OUTZ , , ,0x2D♯ define LIS35_REG_CR1 0x20
,
♯ define LIS35_REG_CR1_XEN 0x1,
♯ define LIS35_REG_CR1_YEN 0x2,
♯ define LIS35_REG_CR1_ZEN 0x4,
♯ define LIS35_REG_CR1_DR_400HZ 0x80,
♯ define LIS35_REG_CR1_ACTIVE 0x40,
♯ define LIS35_REG_CR1_FULL_SCALE 0x20♯ define , , ,OUTX , , ,0X29
,
♯ define , , ,OUTY , , ,0X2B,
♯ define , , ,OUTZ , , ,0X2D,
,,
♯ define , , , , ChipSelectLOW() , , , , HAL_GPIO_WritePin(LIS35DE_CS_GPIO_Port, LIS35DE_CS_Pin, GPIO_PIN_RESET),,
♯ define , , , , ChipSelectHigh() , , , HAL_GPIO_WritePin(LIS35DE_CS_GPIO_Port, LIS35DE_CS_Pin, GPIO_PIN_SET),uint8_t memsc, memsr, memss, memsX, memsY, memsZ,
uint8_t LIS35DE_ReadRegister(uint8_t addr)
,
{,
, , ,uint8_t address = LIS35_READ | LIS35_ADDR_NO_INC | addr,,
, , ,uint8_t data,,
, , ,,
, , ,ChipSelectLOW(),,
, , ,HAL_SPI_Transmit(&,hspi1, &,address, 1, 1000),,
, , ,HAL_SPI_Receive(&,hspi1, &,data, 1, 1000),,
, , ,ChipSelectHigh(),,
, , ,return data,,
},
,,
void LIS35DE_WriteRegister(uint8_t addr, uint8_t data),
{,
, , ,ChipSelectLOW(),,
, , ,uint8_t address = LIS35_WRITE | LIS35_ADDR_NO_INC | addr,,
, , ,HAL_SPI_Transmit(&,hspi1, &,address, 1, 1000),,
, , ,HAL_SPI_Transmit(&,hspi1, &,data, 1, 1000),,
, , ,ChipSelectHigh(),,
}void main(void)
,
{ , , ,,
, , ,// MEMs init , , , , , ,,
, , ,memsc=LIS35_REG_CR1_XEN | LIS35_REG_CR1_YEN | LIS35_REG_CR1_ZEN | LIS35_REG_CR1_ACTIVE,,
, , ,LIS35DE_WriteRegister(LIS35_REG_CR1, memsc), , , ,// Active mode, Enable X, Y, Z,
, , ,memsr = LIS35DE_ReadRegister(CTRL_REG1), , , ,// to verify if the MEMs was configured , , , , , ,,
, , ,,
, , ,MEMS reading,
, , ,// memss = LIS35DE_ReadRegister(STATUS_REG), , , ,// you can check if the data is ready,
, , ,,
, , ,memsX = LIS35DE_ReadRegister(LIS35_REG_OUTX),,
, , ,memsY = LIS35DE_ReadRegister(LIS35_REG_OUTY),,
, , ,memsZ = LIS35DE_ReadRegister(LIS35_REG_OUTZ),,
}We’re moving the ST Community to a new platform to give you a better and more reliable community experience.