2018-02-12 7:43 PM
Board: STEVAL-3DP001 3D Printer Board;
ISSUE: Use a GUI with virtul com port cann't connect the board;
via serial port is possible with ST-LINK on the 3D printer board,
the ST-LINK driver installed,V
irtul com port recognized on PC;
the virtual com port associated with ST-LINK settings is ok;
WIN7 system,have updataed;
the board power is ok;
who can help me to change it, thanks...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.