STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Ecternal interupt occurs 2 times?

Posted on February 19, 2018 at 22:58Hello guys.I've started working with stm32f217zg series and i have a problem with external interupt.I have programmed the mcu and after i push the button the interupt occurs two times instead of one.I use cube mx ...

stm32l073 + LoRa

Posted on February 14, 2018 at 11:19Hello, I'm using stm32l073 + sx1272mb2das for lorawan experiments.my problem is that stm32 board seems to stuck sometimes (in a random fashion). my source code has several timers to manage states of lorawan node (...

Chris Oh by Associate II
  • 4052 Views
  • 8 replies
  • 1 kudos

Resolved! STM32CubeMX ussue

Posted on November 16, 2017 at 09:01 Hi There! Hi have already post this issue but nothing changed from those time. May be i have ''unique'' version of qubeMX but this annoying bug chase me. When I change the Input frequemcy value I get this bug...

0690X0000060PEFQA2.png 0690X0000060PEeQAM.png

VBAT current draw high just after VDD removed

Posted on October 12, 2017 at 03:13 I have a custom circuit board with a STM32F407 part. Everything has worked fine with this board in past revisions, except on the most recent revision we increased the size of the output capacitor on the main regu...

Broken Project from cube v 4.24.0

Posted on January 31, 2018 at 01:46so, i've updated cube to v4.24.0and it starts to make broken .ioc filesi tried several ways to reproduce same issue and here's the problem.1. make a project with stm32f407ze ( not sure it's because of this but.. )2...

STM32F030 TIM16_CH1N and TIM17_CH1N input capture not work

Posted on February 20, 2018 at 10:30Hi,I have configure the TIM16_CH1N and TIM17_CH1N timers as input capture to PB6 and PB7 pin respectively:uint8_t Tim16_17_Init ( void ){    GPIO_InitTypeDef GPIO_InitStructure;    NVIC_InitTypeDef NVIC_InitStruct...

u23 by Senior
  • 2221 Views
  • 3 replies
  • 0 kudos

Resolved! CubeMX 4.24 migrate problem

Posted on January 25, 2018 at 05:11OS: Win10ico version : 4.23 / FW_F4 V1.18.0I can't migrate my project from 4.23 to 4.24. Attach is my ico file.Thank you.

liu yong by Associate II
  • 2626 Views
  • 6 replies
  • 0 kudos

Resolved! CubeMX CAN Config Fails in 4.24

Posted on January 27, 2018 at 08:21Using an STM32L4xx MCU in CubeMX. Enable the CAN peripheral. Go to configuration and click CAN1 ->You'll notice that no dialog box ever appears.Same with migrating an STM32L4xx based project to the new 1.11 framewo...

0690X00000609THQAY.png
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.