2018-02-14 2:19 AM
Hello, I'm using stm32l073 + sx1272mb2das for lorawan experiments.
my problem is that stm32 board seems to stuck sometimes (in a random fashion).
my source code has several timers to manage states of lorawan node (stm32).
maybe the timers stop sometimes because of unknown reasons.
anyone know about this kind of problem?
kind regards.
2018-02-14 2:40 AM
Hi,
Are you using the lorawan stack provided by semtech?
2018-02-14 4:03 AM
my problem is that stm32 board seems to stuck sometimes (in a random fashion)
.
anyone know about this kind of problem?
Surely, this is just a standard software debugging problem?
You need to find out where it is 'stuck', and what makes it 'stick'.
This is why we have things like debuggers, ST-Links, UART trace output, LED diagnostic outputs, etc, etc, ...
http://www.8052.com/faqs/120313
http://www.ganssle.com/articles/developingagoodbedsidemanner.htm
2018-02-14 4:05 AM
nope. source by ST (i-cube_lrwan)
2018-02-14 5:11 AM
I have been working on lorawan node for a long time.
I have always used the stack from here:
https://github.com/Lora-net/LoRaMac-node
You have code example. I never had any problem (on the region tested by them).
2018-02-14 7:05 AM
Well the interrupt priorities and blocking loops in the code could be a problem if you haven't thought about it.
Instrument your code so you understand what's happening internally.
2018-02-21 3:49 AM
Hi, I use Rx continuous mode sometime in source code to get certain packet.
However, I found the device stuck at RX mode and do not capture any packet from random time.
it seems like the device is not in RX mode that time. (and there is no interrupt event such as rxtimeout, rxerror, rxdone)
what is this kind of problem?
by the way, most devices works with no problem but a few have this trouble at random fashion.
maybe there is a problem with RX continuous mode..?
2018-02-21 4:31 AM
Chris Oh wrote:
what is this kind of problem?
It's called a bug. And, as already noted, de-bugging is an essential part of
any
development process - software or otherwise.See the links posted at
https://community.st.com/0D50X00009XkX7ASAV
As
Turvey.Clive.002
said, a standard approach is to instrument your code so that you can see what is (and isn't) happening.most devices works with no problem but a few have this trouble at random fashion.
That is typical of a marginal design; ie, your design is barely within spec - or, possibly, slightly out-of-spec - so that you get away with it most of the time, but it fails when things happen to get a little worse than usual for some reason.
2018-02-21 4:43 AM
The stack has a annoying habit of dwelling in delay loops (or things like TCXO, turning around, sleeping, etc), and blocking in other threads of higher priority, during this time the receiver is NOT listening.
The VCOM code is particularly stupid.
Also make sure the timeout covers both the time between messages, and the time to receive the message. The latter can be quite a long time on high spread factor transmissions. ie when pinging GPS location at top-of-second you want a 1100-1200 ms timeout, setting it to 1000ms inevitably results in loss once it syncs up with the transmitter.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.