STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F429-NUCLEO-144 UART3 IS NOT RECEIVING

Posted on February 21, 2018 at 04:06 Hi, I amUsing STM32F429-NUCLEO- I write the code for UART3 transmit/receive (poling method) and the board is transmitting but the data is not receiving. Pls help me to fix the issue. Find the attached source...

pratheep by Associate II
  • 8169 Views
  • 22 replies
  • 0 kudos

Advice to handle data between Timer IRQ and DMA USART TX IRQ

Posted on February 22, 2018 at 07:46Hello,i am working on a project where i read 4 external adc's in a timer irq and i need to send the data very fast via usart.I know this is achievable only trough DMA USART TX request.The timer irq is executing on...

Bogdan by Senior
  • 756 Views
  • 0 replies
  • 0 kudos

Advice of hardware and software for STM32

Posted on January 14, 2018 at 07:03I am new to this group and wish to start using the STM32 group of MCUs. There seems to be a lot of choice here. Can someone recommend what hardware/software to use in my development. I have used MCUs from Microchip...

martech by Associate II
  • 4919 Views
  • 10 replies
  • 0 kudos

Controlling STM32 via PC

Posted on February 21, 2018 at 17:36Hey. I have program using graphical library SFML on my PC, which is suppose to send commands like 'turn on PWM on pin X', 'set pin X state high' etc to microcontroller. Until now, I was using Raspberry Pi 3 with p...

Resolved! 32F769IDISCOVERY with chip release Z?

Posted on December 23, 2017 at 22:08Does anyone have a discovery board with a STM32F769NI release Z on it?I would like to know if they were already produced because the Ethernet bugin version A is not useful in production equipment.I hope to get a n...

STM32L475VG I2C Rx DMA Problem

Posted on February 21, 2018 at 20:55 Hi i have a big Problem. I have build the HAL with CubeMX 4.24 and i have configured that I2C3 had to Receive 128 Bytes. stm32l4xx_hal_i2c.c static void I2C_ITSlaveCplt(I2C_HandleTypeDef *hi2c, uint32...

Resolved! programmatic reboot of STM32?

Posted on February 21, 2018 at 18:05Hello,Is there a simple way for the program to force a reboot of the STM32 device?  Can I programatically pull the line associated with the reset button low or is there some other way to do a hard reset on the boa...

Library compile error

Posted on February 21, 2018 at 12:47I've included STM32_USB-FS-Device_Driver in my project. When I compile (in IAR) I get a bunch of errorsError[Li006]: duplicate definitions for 'Receive_Buffer'; in 'F:\MotorControlSolution\MultiAxisMotorControl\Ax...

STM32Cube_FW_L4_V1.10.0 : UART Example Not functional

Posted on January 22, 2018 at 10:09Hello,I tried the example UART_TwoBoards_ComPolling from the  STM32Cube_FW_L4_V1.10.0 on the STM32L476RG-Nucleo boards, and it seems it doesn't work as expected.I followed the readme.txt file for the wiring.But i n...

amir by Associate II
  • 2162 Views
  • 4 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.