STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32F410x8 STM32F410xB Datasheet mistakes

Posted on March 07, 2018 at 16:09Hello ST,This datasheet has few mistakeshttp://www.st.com/resource/en/datasheet/stm32f410rb.pdf PC3 is duplicated on this scheme. And also it does not correspond to the pin definition tables below.Please, provide rig...

0690X00000609zvQAA.png 0690X0000060A00QAE.png 0690X00000609uIQAQ.png
Eugene S. by Associate III
  • 1721 Views
  • 2 replies
  • 0 kudos

Resolved! B-L475E-IOT01 Discovery board not listed in STM32CubeMX v4.23

Posted on October 25, 2017 at 23:12Folks -Just updated to STM32Cube_FW_L4_V1.10.0 and STM32CubeMX v4.23.  I can see the B-L475E-IOT01 discovery board and all its' files in the L4 package. I can also select the STM32L475VGTx MCU from the STM32CubeMX ...

questions about stm32vldiscovery

Posted on March 08, 2018 at 14:50hi, may i know for this stm32vldiscovery, whether i could use PA1 and PA2  or PA9 and PA10 for uart communication? because i checked the schematic and datasheet, still not very sure. https://community.st.com/external...

Read from I2C - STM32F767

Posted on March 07, 2018 at 11:52Helo friends.Problem with write on I2C bus I solved. If anyone wanted to, I would provide a solution.Now I have problem with reading. I have got 1 stop bit more.Here is good communication packet.I receive:   S-Addres...

0690X00000609yOQAQ.png 0690X00000609vgQAA.png

STM32L475 Timestamp

Posted on March 08, 2018 at 08:20Hello, I'm developing an application based on STM32L475 device. So I need a timestamp on my application. I saw an RTC_timestamp example of NUCLEO-L476RG. So please anyone can tell how can I port this RTC_timestamp ex...

STM32F102CBT6 USB example

Posted on March 06, 2018 at 04:02Hi, I am working with STM32F102CBT6. And I am going to use USB function of this MCU. Where can I find the suitable examples?Best regards.

Resolved! HAL_UART_Receive() always timeout.

Posted on April 27, 2017 at 06:18Hi all,I met a strange problem that if I input something via a terminal before I call HAL_UART_Receive(); It will always timeout. And it will not recover until I reboot the board.My code is as bellow.  What can I do ...

Bryan Guo by Associate II
  • 10696 Views
  • 9 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.