2018-03-08 7:38 AM
Hi STM community, I want to run valgrind and lint as part of static and dynamic code analysis.
I tried to run valgrind option in system work bench IDE , But it is giving the following error
valgrind: failed to start tool 'memcheck' for platform 'arm-linux': No such file or directory
is there anyway we can fix this issue. I tried one way of fixing by exporting valgrind library path as suggested someone in google.
And regarding the static analysis , I am checking with MISRA with PC-LINT setup, but it is giving errors at standard header files like
'Unable to determine type definition
of intptr_t'So it requires compiler specific option file .
If any such file is available for fixing this issue.
Or any way we can run misra on stm code.
#stm32f7-eval #static-analysis #valgrind2018-03-08 9:28 AM
Valgrind, honestly ?
This would require virtual memory support, and a MMU.
MISRA tools and lint should work, my company uses it for even smaller controllers than Cortex M.
The setup seems a bit tricky, but AKAIK Gimpel (PC-Lint) has a forum, too.
We employ the builtin-MISRA check of the toolchains we use, not for STM32, though.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.