STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Clocksource selection

Hello!I have a question regarding the system clock source selection. Specifically, I would like to understand how the High-Speed External (HSE) clock works. Does the board already include a crystal or ceramic resonator that serves as the source for t...

CPU stalling when erasing FLASH on STM32F405

Posted on July 15, 2016 at 16:13Hello,I have a scenario as follows: I have a Timer 2 that gets interrupted every 1ms. I try to communicate (only Tx) with an external device every 50ms by calling a function inside Timer 2. When the system is running ...

vss01 by Associate II
  • 8057 Views
  • 10 replies
  • 0 kudos

Resolved! STM32F103RBT6 SPI slave mode

Hi ST experts, I'm using STM32F103RBT6, and for GPIO's Alternate functions, I want to use default, not remap.Based on its datasheet, I understand that when its SPI2 interface works in SPI master mode, PB15 acts as data output MOSI and PB14 acts as da...

j2cai by Associate
  • 1216 Views
  • 2 replies
  • 1 kudos

STM32L452 USB virtual com port connect

HelloI have a question. Using the STM32L series, the current USB virtual com port is recognized in the device manager of the PC.Here, I am curious about the maximum number of Com ports that can be connected to the PC.I know that the basic Com port is...

Yoon1983 by Associate II
  • 3541 Views
  • 8 replies
  • 0 kudos

why I can not use LPUART?

I want to communicate with a UART module using an STM32H723 Nucleo board. Receiving data and transmitting over DMA features. İf i choice USART2: PD5 (TX) and PD6 (RX) it works fine? İn same code if change usart2 to lpuart and if i change pins for lpu...

fixaj by Associate II
  • 1496 Views
  • 1 replies
  • 0 kudos

Resolved! STM32N6 with LQFP package?

New question moved from this thread.Hi again, A related follow-up question: Any plans of a N6-version in a LQFP-package this year? Thanks in advance

HAL_SPI_TransmitReceive problems

I am having problems trying to use the HAL_SPI_TransmitReceive function. I am using STM32CubeIDE along with the STM32U5G9J-DK2, I am configuring my side as a full duplex slave using the following parameters:I am working with an embedded processor tha...

Ron54_1-1741900491831.png Ron54_2-1741900774954.png Ron54_3-1741902302260.png
Ron54 by Associate
  • 1476 Views
  • 1 replies
  • 0 kudos

STM32H7 ADC clock prescaler

HelloI'm always confused with the ADC clock config of H7 devices. ok, H7 is not a device for noob but ever after spending days reading datasheets, users manual, appnote, and filling spreadsheets, when starting cube MX, you will always find that the c...

clock cfg.png
tarzan2 by Senior
  • 1327 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.