2025-03-13 1:37 PM
I need to know if this ST i'm using has been made by ST or is a clone
G071GB
GQ28L10
9RCHNB
. 323
Solved! Go to Solution.
2025-03-13 2:43 PM
9R is TSMC Fab 14 in Taiwan, for STMicro
Pull the PCN from Digikey's STM32G071GB page
https://mm.digikey.com/Volume0/opasdata/d220001/medias/docus/6346/Microcontrollers-24-14864.pdf
2025-03-13 2:27 PM
Why you think, its a clone ?
+
What telling CubeProgrammer , after connect ? (show...)
2025-03-13 2:43 PM
9R is TSMC Fab 14 in Taiwan, for STMicro
Pull the PCN from Digikey's STM32G071GB page
https://mm.digikey.com/Volume0/opasdata/d220001/medias/docus/6346/Microcontrollers-24-14864.pdf
2025-03-13 2:44 PM
2025-03-13 2:53 PM
You'd need to work with the vendor more directly to understand if this is the correct firmware, applied appropriately.
You could dump/inspect the FLASH via STM32 Cube Programmer, making sure it's got the binary data, and hasn't written the .HEX as ASCII into the device.
I don't see anything from your presentation so far that the part is not legitimate, but you'd need to check the circuit / PCB to confirm you're working with the right firmware.
2025-03-14 1:15 AM
Dear @Mtrev ,
It can be a change in our bootloader version creating this change at your application level , please check the bootloader version ID between old devices and this new ones check updates in AN2606 and also the version of the devices . Let us know
Ciao
STone-32
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.