STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! can't write to STM32G051G6U6 's flash: PGSERR

Hi community,here my minimal code example: int main(void) { HAL_Init(); SystemClock_Config(); FLASH_EraseInitTypeDef s_eraseinit = {0}; uint32_t pe = 0; s_eraseinit.TypeErase = FLASH_TYPEERASE_PAGES; s_eraseinit.NbPages = 1; ...

ak by Associate II
  • 2013 Views
  • 4 replies
  • 2 kudos

Resolved! How to save app settings to flash

I need to save a couple of bytes (a settings struct) to upper (last) page of the Bank1 flash. The settings are changed very rarely so lifetime of the flash is not an issue. The settings struct has a CSC member so when the settings are read from the f...

Louie88 by Senior II
  • 1734 Views
  • 3 replies
  • 1 kudos

Resolved! STM32U5A5: USB HS without XTAL oscillator - WORKS

Struggling to get my own STM32U5A5 board working... the USB HS PHY was not working, until... (see below).I was confused also with this thread:https://community.st.com/t5/stm32-mcus-products/stm32u5-and-usb-hs/td-p/571774This told me actually as well:...

tjaekel by Lead
  • 5141 Views
  • 6 replies
  • 2 kudos

STM32F4 TIMER AND INTERRUPT

Hello, Can you help me configure cube mx?I would like to make an interrupt on each rising edge of a signal on a gpio,trigger the 16-bit timer on the rising edge and count the number of timer overflowson the signal on another gpio, I don't know how to...

PSEBA.1 by Associate II
  • 950 Views
  • 2 replies
  • 0 kudos

Resolved! Require I/O bank Voltages of STM32N657X0H3Q

Hi All, I was searching for a I/O bank voltages of different GPIO ports available in the controller. In datasheet there is no proper information on supply voltages for the GPIO Pins., could you please suggest the document which is having the informat...

Tejas_P_R_0-1741855315002.png
Tejas_P_R by Associate II
  • 1358 Views
  • 2 replies
  • 1 kudos

Resolved! STM32G431 FDCAN filter doesn't work.

Hi guys. I am using STM32G431KBT MCU. I am using 2 MCU (master / slave) and they communicate via canbus. Canbus is working good but canbus filter is not working. Master canbus address is 0x200 ans slave address is 0x101. I changing master ID (0x150) ...

Cubemx1.png Cubemx2.png
ABURM by Senior
  • 1679 Views
  • 3 replies
  • 3 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.