2020-09-23 3:23 AM
Hi,
We're storing some device configuration on last sector(7) at BANK2 inside internal flash memory. Sometimes device goes into state where part of this this sector is not readable by our code(generates fault) also this sector is not readable by cubeprogrammer and only solution to make our device work again(make unreadable part readable again) is to mass erase chip.
What could be causing such issue where we cannot read only part of flash memory? How can we check why such region is unreadable?
Some more details:
2020-09-23 6:25 AM
I would start by looking at the detail of the fault (hard fault?) to find the source of the issue.
2020-09-23 10:38 PM
We know exactly what's causing fault. We are trying to read from certain address from flash memory(in valid range, not protected by anything).
We tracked down the issue and it seems like problem with timings. What we noticed is that after successfully calling "HAL_FLASH_Program()" and restarting device right after we experience corrupted/damaged flash regions. Shouldn't this function ensure that it is safe to turn off device right after it returns? Adding short delay after programming seems to be solving the issue?
2025-03-13 8:18 AM
Hi, were you able to solve this problem? I encountered the same problem and don’t understand how to solve it
2025-03-13 10:35 AM - edited 2025-03-13 10:39 AM
> Sometimes device goes into state where part of this this sector is not readable by our code(generates fault)
This can occur as result of programming error (for whatever reason) so access to affected flash area triggers ECC errors. This can be cured by erasing the sector properly. This should reset the ECC. If this won't help, erase the whole bank.
Now, why programming errors can occur... For one, because of the "parallelism" parameter too large for available power. Try lesser (slower) values.
2025-03-14 1:59 AM
Thank you, it helped me to clearly indicate the beginning and end of the memory address and setting 2 ways ICACHE; when setting DIRECT MAPPED CACHE, saving occurred with an error
2025-03-14 2:05 AM
@Mike1992 wrote:
Thank you, it helped me to clearly indicate the beginning and end of the memory address and setting 2 ways ICACHE; when setting DIRECT MAPPED CACHE, saving occurred with an error
That's not a STM32H7 product but another MCU part number (maybe H5). If you have an issue please open a new thread an give the part number you are using.
Thanks.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.