STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F405 RTC counting more than 24h!

Posted on April 27, 2018 at 15:47The RTC continues to count after 23:59:59, just changes the day at 39:59:59, what's the problem?I use HAL Library.RTC Output:2018-04-06 weak5, 23:59:572018-04-06 weak5, 23:59:582018-04-06 weak5, 23:59:592018-04-06 we...

Resolved! timer reset counter on falling edge

Posted on April 28, 2018 at 01:37 Hey everyone, I can not seem to get this right and any help would really be appreciated! I'm using a stm32f722ze I have a counter that toggles it's output on every 10th rising clock edge of an external clock ...

0690X00000604cwQAA.jpg 0690X00000604RRQAY.jpg 0690X00000604dVQAQ.jpg
con3 by Senior
  • 1640 Views
  • 2 replies
  • 0 kudos

STM32F103 Maximum input Frequency

Posted on April 28, 2018 at 19:09I use STM32F103 how much is the maximum input maximum encoder frequency. For example if the possible i reading the 20 KHz. I use the TIMER4 encoder mode but i not read the up the 2 KHz. How much is the maximum freque...

Resolved! STM32F767 Nucleo144 - Default clock frequency

Posted on April 28, 2018 at 12:54Hi,what is the default system clock frequency (previous that all clock configuration take place) on the development board 'STM32F767 Nucleo-144'?Where I can find this information?Thank you for the answer.

STM32F427 does not boot after power on

Posted on April 26, 2018 at 17:16Hello,i  am using a design with a STM32F427  100pin package, and notice after leaving the board unpowered for several hours if i power up again, the software its not starting.If i retry the restat the power it will s...

Bogdan by Senior
  • 4235 Views
  • 10 replies
  • 0 kudos

linker script help: What is meant by >RAM_D1 AT> FLASH

Posted on April 28, 2018 at 02:30This follows the .data {....} section.  I think I understand the first part >RAM_D1 meaning the data sections start in the RAM_D1 memory who's origin is 0x240000000 in my case, but what does the AT> Flash do?  My gue...

Erasing chip after Level 2 protection

Posted on April 27, 2018 at 15:00Hi,  I am testing a Nucleo-64 stmL07xxx board and playing around with the protection parts.  After I added my application I set Level 2 protection to prevent read/erase and program of processor. It says its irreversa...

STM32F4 - fastest IIR biquad impelementation in Assembler

Posted on April 27, 2018 at 12:07Hi,I need the fastest implementation of a biquad IIR filter for STM32F4 in assembler. I have to run more than 60 filters at 48kHz. My current best time are 24 cycles per filter with TDF2 (17 at STM32F7).The order of ...

koster by Associate III
  • 1700 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.