can someone say what is the maximum size of EMMC supported in STM32L496
Posted on April 30, 2018 at 11:58I just need to know what is the maximum size of EMMC supported in STM32L496.
Ask questions, find answers, and share insights on STM32 products and their technical features.
Posted on April 30, 2018 at 11:58I just need to know what is the maximum size of EMMC supported in STM32L496.
Posted on April 30, 2018 at 10:38Hi,I'm using STM32F103 board, I connected 8Mhz Quartz crystal to pin PD0 and PD1 ( i.e. OSCIN and OSCOUT). But the oscillator is not working, even I gave supply to Vbat pin.Is their any configuration required I soft...
Posted on February 21, 2018 at 16:20Hi,I have the problem that many of us have as seen on the number of post on the forum. Unfortunatly for me nobody have the same issue as i have!Let s point out first what i'm trying to do.I'm on a small project of...
Posted on April 25, 2018 at 11:09Hello,I found a bug in the latest version of CubeMX which causes the tick timer for HAL to be cleared in code if the corresponding timer pin is cleared.Steps to reproduce:1- Open project with any MCU.2- Configure SYS...
Posted on April 27, 2018 at 14:17The original post was too long to process during our migration. Please click on the attachment to read the original post.
Posted on April 29, 2018 at 20:30Cube MX 4.25Generate source using F446 processor for Atollic TS v9CubeMX and TS are up to dateget following error:..\Drivers\STM32F4xx_HAL_Driver\Src\stm32f4xx_hal_flash_ramfunc.c:163:30: error: expected '=', ',', ';...
Posted on April 29, 2018 at 13:55I am using the Nucleo-64 board F401RE, as the name suggest comes with STM32F401RE.The board doesn't have an external clock (X3 mentioned on the board) and still the HSE RDY register gets enabled , which is actually ...
Posted on April 13, 2018 at 10:39I am firmware engineer. But I am a beginner for ST.I try to get 6 channel ADC 16bit data in high spped by DMA.Now, I have a nucleo-L496ZG board and a TI ADS8364 ADC board.- STM32L496ZG (with FMC)- TI ADS8365 (6 Chann...
Posted on April 29, 2018 at 17:17This problem https://community.st.com/0D50X00009XkWWcSAN by sanjaykumawat8 .In STM32 timer (TIM), when the Update Event is forced by setting TIM_EGR. UG (for example to 'activate' the newly set prescaler value), TIM_...
Posted on April 27, 2018 at 17:49Hi there,I am trying to get my head around the 'new' QSPI Interface, because I never used it before. We are trying to figure out if we can use this interface like a FSMC interface in terms of memory mapping.We are us...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.