2018-04-28 10:09 AM
I use STM32F103 how much is the maximum input maximum encoder frequency. For example if the possible i reading the 20 KHz. I use the TIMER4 encoder mode but i not read the up the 2 KHz. How much is the maximum frequency value?
2018-04-28 11:14 AM
The TIM's should work into the MHz, but don't expect to interrupt at such high rates.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.