STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

USB trace impedance for STM32H725

I am laying out a USB for a STM32H725. I would like clarification on something out of the datasheet (DS13311).Note 2 under table 118 states: No external termination series resistors are required on USB_DP (D+) and USB_DM(D-); the matching impedance i...

VIR by Associate
  • 1035 Views
  • 1 replies
  • 0 kudos

Resolved! NUCLEO-H7S3L8 USB-HS & XSPI problems

  I have several problems with the NUCLEO-H7S3L8 board   1) When initializing the USB - HS peripherals, I getting stuck in the "USB_CoreReset" function: Related problem and after some time when (count > HAL_USB_TIMEOUT) the program goes to Error_Han...

Shpegun60_0-1738247929301.png Shpegun60_1-1738251040439.png Shpegun60_2-1738251337311.png Shpegun60_3-1738251362022.png
Shpegun60 by Associate II
  • 1326 Views
  • 1 replies
  • 0 kudos

Resolved! STM32U585 MPU cacheability?

I am using an STM32U585QI.  I have some memory mapped PSRAM that I'm using.  I have enabled DCACHE, but do I have to manually do something with the MPU for it to cache memory accesses to/from the memory?  The reference manual says:"In addition, the A...

BDoon.1 by Associate III
  • 1255 Views
  • 1 replies
  • 1 kudos

Writing and reading external parallel flash with STM32

HelloI am using STM32F103C8 and I want to read and write to CAT28F010P Flash chip.This flash chip has parallel buses for data and address. Also there are 3 control lines as CE, OE and WE.So there are 28 lines in total coming out of this chip. I was a...

VarioSL by Associate
  • 2427 Views
  • 6 replies
  • 2 kudos

Resolved! Choosing a product

Hi, I find the search system on the ST website to be lacking. There are a lot of parameters I can't search for/filter by. Is there an ST e-mail / form contact I can use to ask for help? If anyone here can help, I'll try to describe what I am looking ...

kasper8 by Associate
  • 940 Views
  • 1 replies
  • 0 kudos

stm32h750vbt6 adc 16bit 14bit issue

Hello,while using this mcu 16bit adc a strange thing happens.the adc signal is test under a sinusoid signal(0.5Hz from a signal generator), and as shown in the figure at certain level adc keeps unchanged, after leaving this level then the signal incr...

mize_0-1723793714498.png mize_1-1723793728792.png mize_2-1723794431864.png mize_3-1723794529822.png
mize by Associate III
  • 7937 Views
  • 13 replies
  • 2 kudos

STM32H743 with USB C connector

Hello there!I've designed a board based on the STM32H743Zit Nucleo board, but unfortunately, I'm facing difficulties with the USB functionality. I'm unsure if it's a matter of configuration or firmware. When I tested USB settings and functionality us...

kmh011 by Associate II
  • 1324 Views
  • 2 replies
  • 0 kudos

Resolved! STM32H743VIT6 USB not working

Hello there! Esteemed ST team member,I hope this message finds you well. I'm reaching out to address an issue I've encountered.I've designed a board based on the STM32H743 Nucleo board, but unfortunately, I'm facing difficulties with the USB function...

Schematic_1.png Schematic_2.png
BrunoS by Associate
  • 3659 Views
  • 2 replies
  • 1 kudos

Why is the DBP bit not set to '1'

Hello, I designed a similar board using STM32H743ZIT6 and STM32H743VIT6. (Rev. V)The board works fine normally.It has been in production for 3 years already. Boards that have already been produced and shipped sometimes become unusable. (since a few m...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.