STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32H7S3L8 SPI Tx DMA burst

Hi,I am trying to use SPI6 transmission with GPDMA on STM32H7S3L8.While Tx transfer works with simple IT handling, it doesn't work with DMA. No way...To take things simple, I am trying a simple burst transfer (I will leave linked list for later), so ...

simo zz by Senior II
  • 1189 Views
  • 2 replies
  • 0 kudos

Resolved! STM32H755 HTRIM PIN high after POR

I'm working with a boost converter and have noticed that when resetting the device a PWM pin remains high/floating for a 100-200msI use the HRTIM with complementary inputs and deadtime insertion.If my lowside pin remains floating/high for an extended...

kip18 by Associate III
  • 826 Views
  • 1 replies
  • 0 kudos

primary bootloader

Hi, I am using the STM32F429ZI microcontroller. I entered primary bootloader mode using the STM32CubeProgrammer option bytes through the ST debugger. My question is: Can I load my LED blinky code (hex file) using the primary bootloader (system bootlo...

kRaje.1 by Associate II
  • 881 Views
  • 1 replies
  • 0 kudos

Resolved! STM32N6 USB device implementation questions

Hello, I have a few questions on STM32N6 capabilities for USB after reading AN4879, AN5967 and RM0486 documents: 1. AN4879 states that to be compliant with the USB 2.0 FS electrical spec, the DP+ pin must be pulled high. Does this also hold true for ...

Send go command to usart bootloader

Hi all,I'm trying to adapt stm32loader python script to use it with stm32wl5 chip. So for now it's working i'm able to flash my stm, but for now after flashing Id like to run my firmware.Here is my step procedure : - Put BOOT0 to 1 - RESET mcu - Put ...

SBaro.11 by Associate III
  • 992 Views
  • 1 replies
  • 0 kudos

Resolved! STM32L496 not raising interruption on USB connection

Hello. I am working on a project that uses a STM32L496VET6 microcontroller and that can work as an USB device. The board has the following usb circuit schematic:The USB signals are connected directly to the MCU (D+ to PA12, D- to PA11, ID to PA10 and...

usb_circuit.png
Mailson97 by Associate II
  • 2114 Views
  • 4 replies
  • 0 kudos

Resolved! DAC in DMA mode @ enabled cache

Hello! A simple question. If I run DAC, using HAL_ADCEx_MultiModeStart_DMA(..., buffer, ...), when D-cache is disabled, I succeed to send what I filled in the buffer. If I do the same with enabled D-cache, I don't succeed. SCB_InvalidateDCache_by_Add...

LeonidP by Associate III
  • 1512 Views
  • 3 replies
  • 3 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.