STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32L051 replacement in LQFP32 with HSE support

Need advice selecting an STM32 device (package should be LQFP32).Want to replace an STM32L051 (LQFP32). Want similar footprint. The replacement shall use less power or equal. Must have possibility to run on an external high speed oscillator (HSE). Th...

MSipo by Senior II
  • 1679 Views
  • 3 replies
  • 3 kudos

Resolved! STM32C071 OSCX_OUT

Under what circumstances is the 32.768kHz clock signal present on the PC15-OSCX_OUT pin of the STM32C071 product?

TG32 by Associate
  • 996 Views
  • 1 replies
  • 0 kudos

Resolved! STM32H573 VFQFPN68 exposed pad details

Hello,We are using the STM32H573 in a new project. We have designed a custom board using the 64-pin LQFP package.The MCU connects to a ethernet PHY using RMII interface.Our product has to meet strict radiated emissions levels that are 7dB lower that ...

benjacam_0-1739447131133.png
benjacam by Associate II
  • 1428 Views
  • 1 replies
  • 0 kudos

STM32L432KBU6TR SPI 16 bit mode issue

STM32L432KBU6 L432 chip, spi3, 16bit mode, 20M baud rate, spi output sclk is 16 cycles when it is powered on again after working for a period of time. Sometimes 15 cycles, sometimes 17 cycles, sometimes 16 cycles are output again. This will help conf...

Pinglei by Associate II
  • 1678 Views
  • 3 replies
  • 1 kudos

Resolved! SMPS Configuration for STM32H7

I've designed a custom board using the STM32H747I MCU, following the STM32H747I-DISCO reference design. In my design, I've connected VLXSMPS to VDDLDO, similar to the reference design. I'm currently setting up the power configuration in STM32CubeIDE ...

KAnahar by Associate III
  • 3417 Views
  • 6 replies
  • 0 kudos

Resolved! STM32F407 Discovery Board UART1 not working

I'm having the same problem on 2 different boards. I gen'd up a simple program using CubeMX and I'm only sending some data to both ports at the same time: void StartTask02(void const * argument) { /* USER CODE BEGIN StartTask02 */ /* Infinite loo...

DS1Z_QuickPrint1.png GPIO STM serial test.jpg

Resolved! SDMMC2 on STM32H755 Nucleo PB14 Reserved

Hi folks,I have SDMMC1 working on CM7 on my H755 Nucleo. Now I want to migrate FAT-FS and the uSD to CM4, in which case I think I should switch to the SDMMC2 peripheral since it's in D2 domain along with CM4.I have a some questions about this and wou...

bramble by Senior
  • 1402 Views
  • 1 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.