2018-05-24 1:03 PM
According with the example these lines of code
#define APPLICATION_ADDRESS (uint32_t)0x08004000
volatile uint32_t *VectorTable = (volatile uint32_t *)0x20000000; uint32_t ui32_VectorIndex = 0; for(ui32_VectorIndex = 0; ui32_VectorIndex < 48; ui32_VectorIndex++) { VectorTable[ui32_VectorIndex] = *(__IO uint32_t*)((uint32_t)APPLICATION_ADDRESS + (ui32_VectorIndex << 2)); } __HAL_RCC_AHB_FORCE_RESET(); __HAL_RCC_SYSCFG_CLK_ENABLE(); __HAL_RCC_AHB_RELEASE_RESET(); __HAL_SYSCFG_REMAPMEMORY_SRAM();work in my SMT32F091RCTx demo board but only with
CubeMX -> SYS -> TimeBase Source -> SysTickIf I chane it in CubeMX -> SYS -> TimeBase Source -> TIM1
the relocated firmware doesn't start.
What have I to do in order to have my relocated firmware working?We’re moving the ST Community to a new platform to give you a better and more reliable community experience.