2018-05-24 11:40 AM
Hi,
I am using Nucleo-144 board connecting UART to my TI device using 250000 baudrate. I always got timeout no matter what timeout using.
Seems the issue is
UART_WaitOnFlagUntilTimeout() failed and return HAL_TIMEOUT.
if(UART_WaitOnFlagUntilTimeout(huart, UART_FLAG_RXNE, RESET, tickstart, Timeout) != HAL_OK)
{ return HAL_TIMEOUT; }while((__HAL_UART_GET_FLAG(huart, Flag) ? SET : RESET) == Status)
#define __HAL_UART_GET_FLAG(__HANDLE__, __FLAG__) (((__HANDLE__)->Instance->ISR & (__FLAG__)) == (__FLAG__))
Above are the code checking timeout.
Reading the HAL user's manual, seems HAL_UART_Receive() need to enable FIFO mode. Is there any reference code to enable FIFO mode or DMA mode? I am using the Cube generated code, and reference to other code. Haven't found any useful example yet.
Thanks,
Dick
2018-05-24 12:16 PM
Suggests it's not actually receiving any usable data, or the ISR is flagging one or more receive errors that need to be cleared.
A basic test would be to loop the TX pin into the RX pin, sending data in the correct form and seeing it be received.
2018-05-24 2:34 PM
I am able to transmit data using HAL_UART_Transmit() function and confirmed the tx/rx data from logic analyzer. Just not get the correct data from HAL_UART_Receive().
2018-05-24 2:43 PM
So look at the USART registers, and reported status/errors. Don't park a debugger 'peripheral view' over the USART register. Read them and print them out a different USART or SWV debug output.
Look at the pin configurations and clocks. Check the RCC and GPIO register bits.
2018-05-24 6:29 PM
I got it now, need to clear some flags. Thx
__HAL_UART_CLEAR_OREFLAG(m_uart_handler);
__HAL_UART_CLEAR_NEFLAG(m_uart_handler);We’re moving the ST Community to a new platform to give you a better and more reliable community experience.