STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Ethernet Packet Broadcast using just MAC address

Posted on June 06, 2018 at 22:00Hello Everyone, I need do a MAC address broadcast of  an ethernet data packet to a network by using the destination address as ff:ff:ff:ff:ff:ff . I don't want to an assign an ip to my devkit. Just want to do a layer ...

STM32H7 set duty cycle of HRTIM1

Posted on September 23, 2017 at 12:32Hello, I am trying STM32H7 HRTIM1, i could set duty cycle and period when i first initialize timer, but after that, i can't change duty cycle. usually, i write direly to compare register, but now it has no effect...

STM32 QSPI MBED

Posted on June 07, 2018 at 16:08Hi I m  working in a project using MBED OS on STM32l433RC, with the aim to use QSPI interface of these board. I integrated some configuration generated by cubeMX but when I running the application nothing hapen when S...

UART DMA not working for some reason

Posted on June 01, 2018 at 17:54Hello again. I've been trying to get my mcu to transfer a buffer via UART to my computer with the help of DMA.for some reason, it does not appear to be working. I think my computer recognizes it correctly just as when...

STM32H7 ADC speed

Posted on September 21, 2017 at 19:46Hello,the STM32H753bi.pdf datasheet Rev1 tells on page 2:3× ADCs with 16-bit max. resolution (14 bits2.7 MSPS, 16 bits 168 kSPS)This would imply a 14-bit SAR adc and 16 bit as a result of oversampling.In chapter...

APB1ENR Power interface clock enable bit

Posted on June 07, 2018 at 09:36I am using stm32F0 and Stm32L0 series MCUs.APB1ENR in Stm32 has Power interface clock enable bit (Bit 28). I have gone through the reference document to unserstand what is its significance.  Bit 28 PWREN: Power interf...

STEVAL-3DP001V1

Posted on June 07, 2018 at 12:45i bought the STEVAL-3DP001V1 for printer 3d last mouth. i got problem with wifi. the webserver not work.it can connect wifi and display. but it can not response any function to the stm chip.  i can't change the ssid a...

Anh Vu by Associate II
  • 795 Views
  • 0 replies
  • 0 kudos

Bug in STM32CUBEMX 4.26

Posted on June 07, 2018 at 09:32Hello,i have updated STM32CubeMx from 4.25.1 to 4.26 and now i can no more generate my project. It freezes during the generation project. I uses a STM32L475.ST, please give me a link to download the 4.25.1 version bec...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.