STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F723EDISCOVERY Demo Source Code

Posted on June 07, 2018 at 17:36Hello,I am looking for the source code to the firmware that comes with the STM32F723 DISCOVERY kit.On the back of the package it says:4/ The demo application software as well as other software examples for exploring t...

J B by Associate
  • 1688 Views
  • 2 replies
  • 0 kudos

STM32F429 & SDRAM

Posted on May 14, 2018 at 17:45Hi,I have been working with a Waveshare Core 429I board, essentially an STM32F429IGT6 & IS42S16400J and Keil.I am trying to store a large array in the SDRAM using the int32_t Array[xxxxx] __attribute__((at(0xD000000)))...

Matt G_2 by Associate
  • 3867 Views
  • 19 replies
  • 0 kudos

STM32CubeMX : USB Mass Storage on NUCLEO-F722ZE STM32F7

Posted on June 07, 2018 at 12:13Hello,I have following things to create .txt on USB Mass Storage (Thumb Drive 32GB)ToolChain:IDE = KEIL MDK 5STM32CubeMX = 4.22.0Middlewares= FATFS and USB_HOSTHardware :NUCLEO-F722ZE STM32F7 Nucleo-144 BoardProject B...

Resolved! CubeF0: Clock mode not configured in LL ADC driver

Posted on May 30, 2018 at 13:38Hi everyone,I'm sorry to push this old thread but I'm facing problems using the LL drivers and initializing the ADC.The function LL_ADC_Init(ADC_TypeDef *ADCx, LL_ADC_InitTypeDef *ADC_InitStruct) doesn't set the CKMODE...

Power line communication

Posted on June 07, 2018 at 17:56Hi all,Anyone is familiar with Powerline Communication with X-NUCLEO-PLM01A1? I was trying to interface the Nucleo board with Arduino R3 and quite a bit stuck. 

IDE settings for HAL without CubeMX

Posted on June 07, 2018 at 17:53Hello everybody! Who created the project using the library HAL without a Cube generator in Atollich TrueStudio? Tell me what settings, I can not configure the project. Also share experience as write projects for stm32...

Hosting by Associate III
  • 778 Views
  • 0 replies
  • 0 kudos

Patch_CubeFW_F3 still have a lot of unused parameter warnings.

Posted on June 07, 2018 at 16:21Hello!I have updated LL drivers for stm32F3. Unfortunately I still get a lot of unused parameter warnings.And I even found one bug.-ThomasThis is a Bug.Must be RTCx->ALRMBR:__STATIC_INLINE void LL_RTC_ALMB_SetDay(RTC_...

T B by Associate II
  • 1050 Views
  • 1 replies
  • 0 kudos

How to use X-CUBE-SPI-EMUL?

Posted on June 07, 2018 at 17:33Hi,  I'm hardware engineer and I'm starting to work with the STM32 µC family so I don't know the environment.I'm already start  a project with CubeMX. I need for my project at least 6 SPI and I use the STM32F407 (onl...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.