2018-06-07 12:32 AM
Hello,
i have updated STM32CubeMx from 4.25.1 to 4.26 and now i can no more generate my project. It freezes during the generation project. I uses a STM32L475.
ST, please give me a link to download the 4.25.1 version because i can't find it anymore.
It's very very very urgent !!! My customer will not wait.
I need to do some modifications today. I tried to phone to my ST contacts but i can't join no one.
Thanks.
Philippe
2018-06-07 12:48 AM
Hello Philippe,
Could you share your ioc please ?
2018-06-07 1:23 AM
For the moment i can't share the ioc file because it's confidential. I must try to reproduce the problem with a simple ioc project.
2018-06-07 2:46 AM
Hi,
i deleted some files in my TrueStudio project folder and now i can generate the STM32CubeMx project.
The files deleted are :
- .mxproject
- common.ftl
- mw_common.ftl
- usbhconf_l4.ftl
- usbhconf_l4.ftl_save
- folder MXTmpFiles
- 2 old log files
I don't know if it is really the origin of the problem.
Philippe
2018-06-07 3:24 AM
OK or you can also share the log file it may be helpful too
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.