STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

MATLAB/Simulink, PIL, .script

Posted on May 03, 2018 at 17:29I am trying PIL in simulink with Nucleo board with stm32. But everytime there is error with crating some file. Does somebody has similar issues? What can be wrong? Simulink model I used is attached.  ### Copy algorithm...

Where Vector Table resides in STMF0 devies

Posted on June 26, 2018 at 14:03I am asking this because when referring to the Reference Manual I see that the vector table resides at addresses 0x0000 0000 to 0x0000 00BC:and the end of the table:But if I go the the linker script file I see that th...

0690X0000060LTpQAM.png 0690X0000060LJRQA2.png

How to load uclinux on STM32F407VET6 controller?

Posted on June 27, 2018 at 13:26Hi,      I have on own board which is having STM32F407VET6 controller.Now I want to add uclinux on my micro controller. Is there any tutorial is available to beginners for load the uclinux on my controller? what are a...

5 minute Timer (LPTIM1) STM32L073

Posted on March 30, 2018 at 10:33Hi everyone, I would like to use LPTIM1 on my STM32L0 to make it wake up (the micro is in Stop Mode) after 5 minutes but I don't know what is the best configuration to do that. Currently I have the configuration belo...

Debugger/ST-Link Utility can not connect to target...

Posted on February 24, 2014 at 15:24Hi ALL.Today I suddenly received a message from the J-Link debugger and from the STLink Utility that I can not connect to target (STM3240G-EVAL board).Any idea what happened? Can I reset the board to its factory p...

magnetron by Associate II
  • 3626 Views
  • 5 replies
  • 1 kudos

STM32F051 adc interrupt problem. Multiple channels.

Posted on June 27, 2018 at 09:27STM32F051 ADC sample 5 channels with interrupt.I'm trying to sample 5 channels using an interrupt. (I'll get to DMA later:0))If I set the sample time to ('ADC_SAMPLETIME_41CYCLES_5') or longer then the code works as e...

Rob1 by Associate II
  • 1233 Views
  • 1 replies
  • 0 kudos

GPIOs or serial shift registers

Posted on June 27, 2018 at 07:33Hi,For an application we need a bulk of digital inputs(comes from sensors- about 30 inputs) and a bulk of digital outputs(go to relays- about 15 outputs). which solution would be better?1- using a high count digital i...

External power supply instead of USB

Posted on June 27, 2018 at 12:01I would like to power my STM32F446RE with an external source instead of using USB. Can I simply switch the position of JP5 such that it is connecting the E5V pin and the middle pin, and then provide the supply to the ...

Solution: longer SPI cables via ''DualSPI''

Posted on June 22, 2018 at 01:12I'd like to share an idea, actually a working solution for a common issue:''Why I cannot use a longer SPI cable?''''How can I make a SPI cable connection longer and keep still a high SPI speed/clock?''Issue:Potentiall...

0690X0000060LN8QAM.png 0690X0000060LD4QAM.png
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.