2018-03-30 1:33 AM
Hi everyone,
I would like to use LPTIM1 on my STM32L0 to make it wake up (the micro is in Stop Mode) after 5 minutes but I don't know what is the best configuration to do that. Currently I have the configuration below.
&sharpinclude 'Lib_Timer.h'
/* USER CODE BEGIN 0 */
/* USER CODE END 0 */
LPTIM_HandleTypeDef lptimHandle;
uint32_t cptCallBack = 0;/* LPTIM1 init function */
void MX_LPTIM1_Init(void){lptimHandle.Instance = LPTIM1;
lptimHandle.Init.Clock.Source = LPTIM_CLOCKSOURCE_APBCLOCK_LPOSC; lptimHandle.Init.Clock.Prescaler = LPTIM_PRESCALER_DIV128; lptimHandle.Init.Trigger.Source = LPTIM_TRIGSOURCE_SOFTWARE; lptimHandle.Init.OutputPolarity = LPTIM_OUTPUTPOLARITY_HIGH; lptimHandle.Init.UpdateMode = LPTIM_UPDATE_IMMEDIATE; lptimHandle.Init.CounterSource = LPTIM_COUNTERSOURCE_INTERNAL; if (HAL_LPTIM_Init(&lptimHandle) != HAL_OK) { _Error_Handler(__FILE__, __LINE__); }}
void HAL_LPTIM_MspInit(LPTIM_HandleTypeDef* lptimHandle)
{if(lptimHandle->Instance==LPTIM1)
{ /* USER CODE BEGIN LPTIM1_MspInit 0 *//* USER CODE END LPTIM1_MspInit 0 */
/* LPTIM1 clock enable */ __HAL_RCC_LPTIM1_CLK_ENABLE();/* LPTIM1 interrupt Init */
HAL_NVIC_SetPriority(LPTIM1_IRQn, 0, 0); HAL_NVIC_EnableIRQ(LPTIM1_IRQn); /* USER CODE BEGIN LPTIM1_MspInit 1 *//* USER CODE END LPTIM1_MspInit 1 */
}}
void HAL_LPTIM_MspDeInit(LPTIM_HandleTypeDef* lptimHandle)
{if(lptimHandle->Instance==LPTIM1)
{ /* USER CODE BEGIN LPTIM1_MspDeInit 0 *//* USER CODE END LPTIM1_MspDeInit 0 */
/* Peripheral clock disable */ __HAL_RCC_LPTIM1_CLK_DISABLE();/* LPTIM1 interrupt Deinit */
HAL_NVIC_DisableIRQ(LPTIM1_IRQn); /* USER CODE BEGIN LPTIM1_MspDeInit 1 *//* USER CODE END LPTIM1_MspDeInit 1 */
}}
void Start_Counter(uint32_t period){
HAL_LPTIM_TimeOut_Start_IT(&lptimHandle, period, 0x0F);}void Stop_Counter( void ){
HAL_LPTIM_Counter_Stop_IT(&lptimHandle);}uint32_t Read_Counter( void ){
return HAL_LPTIM_ReadCounter(&lptimHandle);}void HAL_LPTIM_CompareMatchCallback(LPTIM_HandleTypeDef *hlptim){
cptCallBack++;}uint32_t get_cptCallBack( void ){
return cptCallBack;}I don't know if I use the good callback and the good configuration, currently my callback increase my counter each second, it's too fast (when I call '
Start_Counter' I put period = 0xFFFFF).
Have you any ideas or advices ?Thank's a lot
Regards
Simon#deepsleep #stm32l073 #stm32l073rz #lptim #stopmode2018-03-30 3:00 AM
Hello Simon
You can take a look into your local Cube repository for STOP with RTC autowakeup example:
\STM32Cube_FW_L0_V1.10.0\Projects\STM32L073RZ-Nucleo\Examples\PWR\PWR_STOP_RTC
Regards,
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2018-03-30 4:51 AM
lptimHandle.Init.Clock.Source = LPTIM_CLOCKSOURCE_APBCLOCK_LPOSC;
lptimHandle.Init.Clock.Prescaler = LPTIM_PRESCALER_DIV128;So, as it appears that you did not change the default value of RCC_CCIPR.LPTIM1SEL, what's your APB clock frequency? Divide that by 128 and the autoreload value, which is
it's too fast (when I call '
Start_Counter' I put period = 0xFFFFF)
oh, the LPTIM is 16-bit only, so you can't set it to 0xFFFFF.
JW
2018-03-30 8:07 AM
take a look at its prescaler and timer width and see if you can achieve the said duration with just the prescaler + timer period.
if not, consider a different timer that can;
if this timer is your only option, set up the mcu to wake up at certain interval, like roll-over. In the isr, increment a counter and test if certain number of roll-overs has been achieved. Essentially that counter forms your most significant bits of the timer.
2018-06-27 3:50 AM
any idea how i can configure the LPTim for period hour please , and any solution for period in minutes please
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.