STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Failsafe upgrades with STM32L476 Dfu

Posted on June 27, 2018 at 15:24On the STM32L476, we have been using the Dfu program that comes loaded in system memory.We've been using this ROM code succesfully as a way to load firmware on to the MCU flash over USB, with the documented Dfu file f...

Why does STM32Cube recommend to not use SysTick

Posted on June 27, 2018 at 22:08as TimeBase Source?Today, I've been trying to activate FreeRTOS' USE_TICKLESS_IDLE feature.It turns out that the tickless idle --in fact it is a unnecessary tick suppression-- works only when Timebase Source is SysTic...

cube_mx 4.26.0+STM32Cube FW_F4 V1.21.0ç�?Ÿæˆ�的代ç �编译ä¸�通过

Posted on June 28, 2018 at 05:54cube_mx 4.26.0+STM32Cube FW_F4 V1.21.0,一但使能了sd�?�+fatfs+freertos�?�,生�?的代�?就编译失败。麻烦修正一下,谢谢。编译报错:这里�?�有两个问题:1.main.h循环包�?�。�?�: main.h-->#include ''stm32f4xx_hal.h'' --> #include ''stm32f4xx_hal_conf.h''-->#include ''m...

0690X0000060LUsQAM.png

Resolved! STM32F4cube examples - but where ?

Posted on June 27, 2018 at 16:17Dear Community,I’ve just installed the STM32F4cube from SetupSTM32CubeMX-4.26.0.exe  but I cannot find the “Hundreds of examples for easy understandingâ€� mentioned on https://www.st.com/en/embedded-software/stm32...

M G_2 by Associate III
  • 1923 Views
  • 2 replies
  • 0 kudos

STM32F765 to eMMC integration issues

Posted on May 17, 2018 at 10:04 Dear All We are facing some issues on eMMC integration with STM32F765 micro controller , In STM32CUBE we generated SDIO interface source code , eMMC manufacture is says this source code was SDcard interface. How we...

nagaraj by Associate II
  • 6999 Views
  • 14 replies
  • 0 kudos

auto-install.xml for STM2CubeProgrammer

Posted on June 27, 2018 at 19:22I save lots of time using the automatic installation feature of STM32CubeMX, as I simply provide the STM32CubeMX installer with this XML file:<?xml version='1.0' encoding='UTF-8' standalone='no'?><AutomatedInstallatio...

Resolved! STM32WB : ''stm32cubemx cannot load this mcu''

Posted on June 26, 2018 at 09:25Helloi try to load STM32WB MPU into STM32CubeMX but i get the following error (by double click on any of STM32WBB55CG RG or VG) :'stm32cubemx cannot load this mcu'stm32cubemxversion is 4.26.0 Cube V1.0have you any ide...

STM32Cube MX Project Build Problem

Posted on June 27, 2018 at 17:03STM32Cube MX Project Build Problem I'm having a build problem with a project brought over from STM32CubeMX with a -F072RB chip. After opening the project in True Studio and building (clean) I find the following error ...

I2C Timing Calculation

Posted on June 27, 2018 at 05:32Hi Everyone,I am working on I2C to sense DAC data. I generated the code using STM32CubeMX. It gives timing in hex format i.e.'hi2c2.Init.Timing = 0x10707DBC;'. It does confuse me that how does it calculate timing ? I ...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.