STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32H7S7Z8J6 XSPI1 interface

Hi all,We have a question regarding the external memory interface connected to XSPI1 on the STM32H7S7Z8J6. We use the APS6404L-3SQN-ZR 64Mb external ram. We activated the XSPI interface with the following parameters:We also created the memory partion...

XSPI1 settings.png XSPI1 partition.png
leddel32 by Associate II
  • 668 Views
  • 1 replies
  • 0 kudos

Resolved! RTC LSE not working on power off with Vbat

I'm using the stm23F103C8 and I would use the RTC internal cloak/calendar. The program is working fine and I have used the LSE osc (32KHz..) as clock source. I have connected a 3V battery to the VBAT pin. My problem is that the switching off the main...

OldSTMan by Associate II
  • 6849 Views
  • 10 replies
  • 1 kudos

Resolved! STM32H743VG Pin PC2_C and PC3_C

Hello folks!The STM32H743VC Processor has two pins, that have a "_C" at the end of the name:Pin 17: "PC2_C" and Pin 18: "PC3_C" When I want to know what the C means, the Datasheet  says: refer to the reference manual.DS12110 Rev 10 - page 67 - Pin De...

a.png
CBerg by Senior II
  • 2946 Views
  • 6 replies
  • 4 kudos

I3C Ctrl Transmit question

Hello,I am working with the STM32H503CBT6 and using the I3C Transmit_IT in Controller mode for communication.However, I encountered a problem, when I sent more than 260+ bytes, the data sent by the logic analyzer to capture, found that the captured d...

hancheng by Associate
  • 661 Views
  • 0 replies
  • 0 kudos

STM32N657X0 with self powered USB-C port

I am designing an STM32N657X0 based custom PCB which has a USB Type C port. The USB device would be self- powered, i.e, it will not be powered from VBUS. The intended use of this port is to plug the PCB to a host PC, similar to USB flash drive for da...

Resolved! Workshop and training material on STM32N6 please

Hi,The recent webinar with your partner Edge Impulse on 26th March was useful to taste the capabilities of STM32N6. Until now in my previous STM32 MCU projects are built with ST official tools like STM32CubeMX. But there is no much information availa...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.