STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

I2C clock not generated on SCK pin

I was working on i2c using STM32L476 nucleo board.I used stm32cube to make a code for keil.When I generated the code and programmed it in the board i found that the oscilloscope was not showing any clock on it .Oscilloscope's channel1 was connected t...

USB Stall Behavior (CubeMx, CDC)

Hi,I'm struggling to integrate a USB interface into a bootloader. The microcontroller always stalls the USB communication. To find the cause of this problem I have set up a simple project to compare the USB transfers and came to a point where I can't...

0690X0000060OGFQA2.png 0690X0000060OGPQA2.png

STM32L4 nucleo board programming problem

I have a STM32L476RG nucleo board.Recently when I tried to program it using keil I found some error messages and I was unable to program it.I found that LD3 LED is glowing .Initially when the board was programmable it was not glowing.I am attaching e...

0690X0000060OTCQA2.png 0690X0000060OT7QAM.png

Steps to have external SDRAM work properly!

I'm editing linker and startup files according to the example "FMC_SDRAM_DataMemory" but i con not access SDRAM. In example, it has only 2 regions as FLASH and RAM but we have 5 regions as FLASH, DTCMRAM, SRAM1, SRAM2 and MEMORY_B1. Also how can an i...

N ORhan by Associate III
  • 1233 Views
  • 2 replies
  • 0 kudos

On STM32F4 discovery board we got accurate 7000 adc sampes but unable to read 7000 adc samples using stm32f030r8 using SPI. Please provide your inputs.

Hi,We are using ADS1292 to get the ADC samples and we had successfully read the 7000 sample with the help of imx6 processor, STM32F4 controller.But now our project requirement changed and we have to use the STM32F030R8 controller with same ads1292 bo...

Bhushan by Associate II
  • 1530 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.