2018-07-27 12:26 AM
My device is STM32F051R8T6, the same used in STM32F0 discovery board.
I was tweaking with the clock configuration section to try different clock configurations like HSI and HSE, etc. I could erase, flash and verify the program successfully, however the output doesn't seem to work as expected. So, i tried a simple GPIO pin toggle in program and flashed it successfully to the chip, still the output didn't change/work at all. I flashed the same program into my stm32f0 discovery board and the output worked fine. What might have happened to the STM32F051R8 chip? I guess I might have bricked the device, because of the clock tweaks.
How do I resolve this issue? How do I prevent this from happening in the future.
Any valid inputs will be of great help.
Thanks.
2018-07-27 2:41 AM
A quick update!
The program works fine when in debug mode. But as soon as I stop the debugger, the program stops executing. What could be the problem?
2018-07-27 5:30 AM
is Boot0 low or High ?
I tie it low with 10K, to always boot from user flash
2018-07-27 5:33 AM
in Visual studio, if I stop debugging, the Processor is locked at stop or break, I guess.
I have to power off to release the SWD, then the board reboots from user flash when the power is reapplied.
2018-07-27 9:59 PM
Yes, the BOOT0 pin is pulled low with 10K resistor. I was tweaking the clock configuration, I read somewhere that it can brick the device. Now, does it have anything to do with flash bootloader concept?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.