STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

VCC-GND STM32F407VET6 Mini Board

Posted on August 22, 2016 at 21:12 Posting some resources for this neat little breakout board from https://vcc-gnd.world.taobao.com/, also available in an STM32F103VET6 model, the schematic is one for a slightly older F103 variant. ...

0690X00000603BaQAI.jpg 0690X00000603BfQAI.jpg

Nucleo-L4R5ZI USB CDC

Dear All,I would like to ask how to manage USB CDC on the nucleo-l4r5zi board. I would like to send data from a uC to the PC via USB.The main function looks like that:int main(void){ HAL_Init(); SystemClock_Config(); MX_GPIO_Init(); MX_USB_DEVICE_Ini...

mike by Associate
  • 1010 Views
  • 1 replies
  • 0 kudos

Resolved! My Nucleo-L152Re not connected by USART2 to PuTTY

Hello!​I try to print message from my Nucleo-L152RE board by USART2 to PuTTY, but see only black screen without symbols. On other side, my Windows 10 see Virtual COM and I can to burn the code to Nucleo board from EWARM​. What I must to do to solve ...

Max75 by Associate II
  • 6201 Views
  • 8 replies
  • 0 kudos

Compiling error.

Hi.Have you ever compile code with error: More than one section matches selector - cannot all be FIRST/LAST.I searching on google I see that the error because when appear two file same startup_stm32f746xx.s in Startup file and Divice File. I'm delete...

How to Trigger TIM2 via TIM3?

Hi. I'm reading Incremental Optic encoder with Timer3. The counter value is 4095 when the encoder rotates one turn. My goal is to produce pulses from 0-25ms through another timer when the Encoder turns half a turn. In order to do this, I am trying t...

STM32F051R8 not working after clock configuration

My device STM32F051R8 used to work without any issues prior to this. I was working with internal RC till then, and wanted to experiment with different clock source(HSE) and was trying out a code. It so happened that after flashing that code the devic...

STM32F7 (Nucleo F767I) Ethernet Linkup Problem

Hello,I have generated sample project with latest STM32Cube for NUCLEO F767I and have ethernet linkup problems... (don't work)I have generated the same sample for NUCLEO F429ZI and working fine ! STM32F779I-EVAL (but here ist other MII PHY ) and work...

maniek by Associate III
  • 959 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.