2021-02-12 6:29 AM
int main(void)
{
/* USER CODE BEGIN 1 */
arm_cfft_radix4_instance_f32 S;
float32_t maxValue;
uint32_t maxIndex;
uint16_t i;
uint16_t height[128];
/* USER CODE END 1 */
/* MCU Configuration--------------------------------------------------------*/
/* Reset of all peripherals, Initializes the Flash interface and the Systick. */
HAL_Init();
/* USER CODE BEGIN Init */
/* USER CODE END Init */
/* Configure the system clock */
SystemClock_Config();
/* USER CODE BEGIN SysInit */
/* USER CODE END SysInit */
/* Initialize all configured peripherals */
MX_GPIO_Init();
MX_DAC_Init();
MX_TIM2_Init();
MX_I2S3_Init();
/* USER CODE BEGIN 2 */
HAL_Delay(100);
HAL_TIM_Base_Start_IT(&htim2);
/* USER CODE END 2 */
/* Infinite loop */
/* USER CODE BEGIN WHILE */
while (1)
{
/* USER CODE END WHILE */
/* USER CODE BEGIN 3 */
HAL_I2S_Receive(&hi2s3,(uint16_t *)buffer,512,100);
// for(uint16_t y=0;y<SAMPLES;y++)
// {
// buffer[y] >>= 14;
// }
for (i = 0; i < SAMPLES; i++) {
Input[(uint16_t)i] = (float32_t)((buffer[i] - (float32_t)16777215.0) / (float32_t)16777215.0);
// Input[(uint16_t)(i+1)] = 0;
}
arm_cfft_radix4_init_f32(&S, FFT_SIZE, 0, 1);
arm_cfft_radix4_f32(&S, Input);
arm_cmplx_mag_f32(Input, Output, FFT_SIZE);
arm_max_f32(Output, FFT_SIZE, &maxValue, &maxIndex);
for(uint16_t k=0;k<FFT_SIZE/2;k++)
{
deger[k]=(float32_t)Output[k];
}
}
/* USER CODE END 3 */
}
/**
* @brief System Clock Configuration
* @retval None
*/
void SystemClock_Config(void)
{
RCC_OscInitTypeDef RCC_OscInitStruct = {0};
RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};
RCC_PeriphCLKInitTypeDef PeriphClkInitStruct = {0};
/** Configure the main internal regulator output voltage
*/
__HAL_RCC_PWR_CLK_ENABLE();
__HAL_PWR_VOLTAGESCALING_CONFIG(PWR_REGULATOR_VOLTAGE_SCALE1);
/** Initializes the CPU, AHB and APB busses clocks
*/
RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSE;
RCC_OscInitStruct.HSEState = RCC_HSE_ON;
RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;
RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSE;
RCC_OscInitStruct.PLL.PLLM = 4;
RCC_OscInitStruct.PLL.PLLN = 168;
RCC_OscInitStruct.PLL.PLLP = RCC_PLLP_DIV2;
RCC_OscInitStruct.PLL.PLLQ = 7;
if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
{
Error_Handler();
}
/** Initializes the CPU, AHB and APB busses clocks
*/
RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK
|RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2;
RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK;
RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1;
RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV4;
RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV2;
if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_5) != HAL_OK)
{
Error_Handler();
}
PeriphClkInitStruct.PeriphClockSelection = RCC_PERIPHCLK_I2S;
PeriphClkInitStruct.PLLI2S.PLLI2SN = 98;
PeriphClkInitStruct.PLLI2S.PLLI2SR = 2;
if (HAL_RCCEx_PeriphCLKConfig(&PeriphClkInitStruct) != HAL_OK)
{
Error_Handler();
}
}
/**
* @brief DAC Initialization Function
* @param None
* @retval None
*/
static void MX_DAC_Init(void)
{
/* USER CODE BEGIN DAC_Init 0 */
/* USER CODE END DAC_Init 0 */
DAC_ChannelConfTypeDef sConfig = {0};
/* USER CODE BEGIN DAC_Init 1 */
/* USER CODE END DAC_Init 1 */
/** DAC Initialization
*/
hdac.Instance = DAC;
if (HAL_DAC_Init(&hdac) != HAL_OK)
{
Error_Handler();
}
/** DAC channel OUT1 config
*/
sConfig.DAC_Trigger = DAC_TRIGGER_NONE;
sConfig.DAC_OutputBuffer = DAC_OUTPUTBUFFER_ENABLE;
if (HAL_DAC_ConfigChannel(&hdac, &sConfig, DAC_CHANNEL_1) != HAL_OK)
{
Error_Handler();
}
/* USER CODE BEGIN DAC_Init 2 */
/* USER CODE END DAC_Init 2 */
}
/**
* @brief I2S3 Initialization Function
* @param None
* @retval None
*/
static void MX_I2S3_Init(void)
{
/* USER CODE BEGIN I2S3_Init 0 */
/* USER CODE END I2S3_Init 0 */
/* USER CODE BEGIN I2S3_Init 1 */
/* USER CODE END I2S3_Init 1 */
hi2s3.Instance = SPI3;
hi2s3.Init.Mode = I2S_MODE_MASTER_RX;
hi2s3.Init.Standard = I2S_STANDARD_MSB;
hi2s3.Init.DataFormat = I2S_DATAFORMAT_24B;
hi2s3.Init.MCLKOutput = I2S_MCLKOUTPUT_DISABLE;
hi2s3.Init.AudioFreq = I2S_AUDIOFREQ_44K;
hi2s3.Init.CPOL = I2S_CPOL_LOW;
hi2s3.Init.ClockSource = I2S_CLOCK_PLL;
hi2s3.Init.FullDuplexMode = I2S_FULLDUPLEXMODE_DISABLE;
if (HAL_I2S_Init(&hi2s3) != HAL_OK)
{
Error_Handler();
}
/* USER CODE BEGIN I2S3_Init 2 */
/* USER CODE END I2S3_Init 2 */
}I am trying to read data from INMP441 mems sensor with I2S protocol with stm32f407 discovery, with 24bit 32 frame configuration at 44khz, but I think I have a problem in reading my codes above, can you help me?
2021-02-12 10:24 AM
Hello
A value 96 to PLLI2S.PLLI2SN gives less clock error than 98. (for 44kHz clock freq)
>>HAL_I2S_Receive(&hi2s3,(uint16_t *)buffer,512,100);
this function asks for 256 samples. Is SAMPLES 256?
2021-02-20 3:43 AM
As you said, I ran it at 96 Mhz. My problem is solved. I concluded the process by reading 2 times in I2S and combining 16-bit data. Thank you.
2025-04-02 5:27 PM
I am running into the same problem and I have been trying to read 2 times in I2S and combining 16-bit data with this line, and then extract the first 24 bits from the combined 32-bit data. However, so far the audio that I extracted is still quite distorted. Would you mind sharing more details onto how you got the right audio? Thank you so much!
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.