STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

DMA STM32L0 operation

Hello. I am using STM32L053R8T6. I connect 3 ADC channels (PA4, PA6, PA7). For this I use DMA. I need the resolution of the ADC - 8 bits, for this I initialize an array with the dimension of 8 bits (volatile uint8_t AdcValue [3];)I am using DMA HAL_A...

0690X000006CFEfQAO.png
ABoga by Associate
  • 969 Views
  • 1 replies
  • 0 kudos

HardFault exception problem

I make boot loader for jump to 0x08020000And, I make program that start from 0x08020000, also same vector table address(0x08020000)It works well, but sometimes(when program modified), it doesn't workI use debugger, and get result below//Fault excepti...

0690X000006CFCoQAO.jpg
mcho.19 by Associate II
  • 5506 Views
  • 8 replies
  • 0 kudos

STM32F446RE I2S can't output clock

hi all, I wan to use PA4, PA5 and PA7 as I2S.but can't output clk. follow is code for I2S setting: // clock setting   RCC_PLLI2SConfig(16, 334, 2, 7, 7);  RCC_I2SCLKConfig(RCC_I2SBus_APB1, RCC_I2SCLKSource_PLLI2S);  //RCC_I2SCLKConfig(RCC_I2SBus_APB2...

khuan.81 by Associate
  • 2251 Views
  • 6 replies
  • 0 kudos

Is it possible to configure the IWDG timer to 30 minutes?

I have an IoT hardware (using STM32L152) that carry out some tasks and go to STOP mode for 30 minutes. Then, it will wake up and repeat the same process again. Now, I would like to add the watchdog timer to ensure everything works fine. My question i...

Khoo.B by Associate III
  • 2681 Views
  • 5 replies
  • 0 kudos

STM32F746 LwiP-Ethernet Buffers shift in SRAM memory

Hallo everybody,I use a NUCLEO STM32F746 board and playing with an LWIP echoclient example.Everything is working as expected.However if I shift the .RxDecripSection and .TxDescripSection from the 0x20010000 and 0x20010080 addresses to the 0x20030000...

STM32H743VITx DCMI DMA Capture in RAM_D2

Hi, i able to trigger BSP_CAMERA_SnapshotStart and save the camera output to RAM_D1. But when i change to save the camera output to RAM_D2. I not able to get the output at BSP_CAMERA_FrameEventCallback.//uint8_t camera_frame_buffer[480*480] __attribu...

KK by Associate II
  • 2335 Views
  • 3 replies
  • 0 kudos

Resolved! Where is timer clock source documented?

For example timer A: is it low-speed (APB1) 'APB1 timer clock' or high-speed APB2 'APB2 timer clock'?I read the timer and RCC sections but could not figure this out...Can you tell me where this is documented?Thanks!

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.