2025-04-15 1:32 AM
This is the output from an UPS inverter. they are driving signals of four mosfets of H-Bridge.
I can generate same signals using stm32f103 advanced motor conotrol timer(TIM1).
center aligned pwm and complimentary output with maximum 20us dead time.
The problem is, stm32f103 cant give more than 20us dead time. But i need 100us for my project.
Is there any other way to generate these signals ?
Thanks
2025-04-15 3:12 AM
Hello @jubaid_h,
Consider using STM32G474 with more advanced timer features and precise control of dead time through HRTIM!
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2025-04-15 3:23 AM - edited 2025-04-15 3:24 AM
its not possible to change the device right now. is there any other way like configuring several timers ?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.