STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Brown Out Reset does not work

Hello,we have a pcb with an STM32F765VIT6 on it. Everything works nicely except that there are unfrequent bit flips in the flash after disconnect and connecting the power supply..We tried to activate the brown out reset in software but after measurin...

Andreas1 by Associate II
  • 4129 Views
  • 6 replies
  • 0 kudos

RTC Running only in Debug Mode

Hi,I had generated RTC code for STM32L072CZ using cubemx, I'm reading the time and sending data via uart, when I'm in debug mode i can able to see the time via UART and when i stop debug mode then timer doesn't increment instead the initial value is ...

I couldnt find "output folder options" in the <ST Motor Control Workbench> in my computer. Is it because of the new Version of this Workbench ?

Im supposed to use STSW-SPIN3201 firmware with board STEVAL-SPIN3201 to control a 3-phase permanent magnet motor with Hallsensor ST Motor Control Workbench. For that i need to use <ST Motor Control Workbench>. For my further application with this Wor...

AAire by Associate
  • 690 Views
  • 0 replies
  • 0 kudos

STM32Fx external input counting and triggering ADC

Hi,I have a PWM signal input to STM32Fx MCU, I would like to count the number of pulses and trigger ADC on each rising edge of the PWM.If I use the input as the clock source for the Timer I don't know how to generate a trigger to the ADC on each puls...

priven by Associate II
  • 2925 Views
  • 6 replies
  • 0 kudos

USART in SPI mode

Is it possible to configure the USART as SPI master, with SPI slave having 16 bit data frames (AD5592R) ?

EE_CV by Associate II
  • 7568 Views
  • 10 replies
  • 0 kudos

Is there a conflict between Timer 2 and I2C in STM32F103?

Hi. I'm using an MPU (6050), an encoder (AS5048A) and STM32F103. For the MPU I am using the I2C protocol, for the encoder (works through the pwm) the Timer2 and its interruption are used. The I2C only works if no encoder readings are being made. Is t...

FVasc by Associate
  • 1477 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.