STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32 Bootloader size

Dear All,I am going to use stm32f030f4 which has 16K flash & 4K SRAM. if I use STM32 bootloader , will Bootloader reduce available Flash/Ram or there is other reserved section for Bootloader i mean that i would like to save all flash/ram space for my...

AMost by Associate
  • 1870 Views
  • 3 replies
  • 0 kudos

Does the STM32H750 support multi-drop SWD?

Does the new STM32H750 MCU Family include the ARM CoreSight Serial Wire protocol version 2 in ADIv5.1 released in Sept 2009 which permits support for the multi-drop SWD extensions? The objective being the use of a single SWD debug header to enable de...

GGonz by Associate
  • 2701 Views
  • 3 replies
  • 1 kudos

Sample codes for STM32F051C6

Dear sir/madam,I want sample codes for this controller i.e. STM32F051C6. Please provide the sample codes for following parameters.TimerPWMDACDisplay 8x2Thanks and Regards,Thippeswamy H U

TH U by Associate
  • 2029 Views
  • 3 replies
  • 0 kudos

How to reconfigure STM32L476 after exit standby mode

Posted on May 24, 2017 at 15:34Hi,We are working with SensorTile (STM32L476). To reduce power consumption, we are using the standby mode with sram2 retention. Our intention is to configure BlueNRG-MS (with advertising enabled), enter standby mode an...

Resolved! The problem with the i2c interface on the controller stm32f103

I have a problem with the operation of the I2C interface on stm32f103. Hangs waiting for ADDR bit(while(!(I2C1->SR1 & I2C_SR1_ADDR))) in the master transmit mode.In the Internet, many people have this problem, but is no solution. Who was the problem...

Hosting by Associate III
  • 2201 Views
  • 3 replies
  • 0 kudos

Tracealyzer in STOP mode

Hi,I have question about streaming data to Percepio TraceAlyzer when the MCU is in Tickless mode - in my case in STOP mode (main clock is stoped). I use FreeRTOS and STM32L152VB. My application periodically wakes up with period T=1.5 s. I use for tim...

JAN R by Associate III
  • 2485 Views
  • 5 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.