2019-02-05 2:23 AM
Hi,
I had generated RTC code for STM32L072CZ using cubemx, I'm reading the time and sending data via uart, when I'm in debug mode i can able to see the time via UART and when i stop debug mode then timer doesn't increment instead the initial value is transmitted continuously.
Thanks & Regards,
Vijay Rakesh.
while(1)
{
HAL_RTC_GetTime(&hrtc,&Time,RTC_FORMAT_BIN);
sprintf(Buff,"Time : %d:%d:%d\n",Time.Hours,Time.Minutes,Time.Seconds);
HAL_UART_Transmit(&huart2,(uint8_t *)Buff,strlen((const char*)Buff),500);
HAL_Delay(1000);
}
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.