STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32L0 Cannot wakeup from STOP with LPTIM IRQ ?

Posted on September 21, 2017 at 13:00 Hello, I'm trying to wake up from STOP mode using LPTIMer on STM32L LPTIM is clocked by LSE(32K) used as a simple upcounter, and I'm using both ARR and CMP Interrupts from LPTIM, so corresponding bits a...

laurent1 by Associate
  • 1260 Views
  • 1 replies
  • 0 kudos

which of the flags I need to turn on and which header files I need to include in the firmware code to enable the sdcard mode of MCU on ?

Hi. I want to write a dummy file in sdcard. I am done with the code but I would like to know which of the flags I need to turn on and which header files I need to include in the firmware code to enable the sdcard mode of MCU on for Input Output opera...

SSD1963 and FSMC problems

Hello, I have some TFT screens with SSD1963 (4.3 - 5 - 7 inch)I'm using them with stemwin and stm32f407 board. All is working but 4.3 and 5 inch become white screen after a while (time is random). 7inch is working perfect. Firstly I made FSMC setting...

AULUS.10 by Associate
  • 1049 Views
  • 1 replies
  • 0 kudos

Resolved! STM32F302CB Problems with USB

Posted on April 05, 2018 at 12:22Hi,I'm trying make USB custom HID with stm32f302CB. I'm using Keil v5.23 and STM32CubeMX. The problem: PC just don't recognize the USB, when i running in debug mode i saw something strange. Just after calling HAL_PCD...

0690X0000060ARLQA2.png 0690X0000060ARQQA2.png 0690X0000060ARVQA2.png 0690X0000060ARpQAM.png

Am I correctly setting up TIM2 input capture?

Hi everyone.I'm trying to setup TIM2_CH4 remapped as input capture, in order to detect rising edges on PB11.I'm working with HALs. And my code is next:First of all, for initialization: // APB2 (which is 64 MHz) at 8 MHz timer_cap_timhandle_.Inst...

0690X000006DMgfQAG.png
areify by Associate II
  • 941 Views
  • 0 replies
  • 0 kudos

CubeMX 4.25 ToolChain Location Bug ??

Posted on March 26, 2018 at 20:32In CubeMX 4.25.0:      Project -> Settings  (or just Alt-P):    shows Project and ToolchainFolder locations:     But the project name get appended to these locations every time you enter the settings panel, so the co...

Goof Ball by Associate III
  • 2715 Views
  • 4 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.