STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

devnonce is too small

hi guys,I am experiencing an issue related to the "devnonce is too small" error. When I attempt to switch end nodes in the TTN network, I change the end node network keys (such as Join EUI, Dev EUI, and App Key) through USART. I stop the LoRa MAC, de...

kRaje.1 by Associate II
  • 929 Views
  • 1 replies
  • 0 kudos

STM32G4 UCPD:Debug issue

Hello, I have encountered a similar problem to the one in this link .I am also trying to use the UCPD Monitor to send message. For example, I request a new voltage from the source using the "Request Power Profile" message from the "Message Selector" ...

Susu_0-1741242599589.png Susu_1-1741242623726.png
Susu by Associate II
  • 2767 Views
  • 5 replies
  • 0 kudos

GPDMA Queues & Nodes

Hello,  Does someone have information, project, whatever that can help me understand how do the Queues and Nodes work and interact with each other?  My STM32 has two ADCs, ADC1 & ADC4, and i want to trigger both of them to read values comming from mu...

Marc3 by Associate III
  • 1303 Views
  • 1 replies
  • 0 kudos

STM32G0B1X RTC_OUTPUT generated at ADC_IN pin number PA4

Hi team,I am using STM32G0B1 for my project development were I use PA4 as a ADC_IN in analog mode and using RTC for date and time setting, though I am not using(/set) RTC_OUT but  1 Hz RTC calibration output getting activated at power on or at rebbot...

st21 by Associate II
  • 2328 Views
  • 8 replies
  • 0 kudos

Issue with configuring a pin to output high level with STM32H563

需要寻求帮助,我使用STM32H563VIT6配置了一个引脚输出高低电平,在debug模式下可以运行,在正常运行(release)下就不能得到结果,这是为什么?而且我是在HSE不行还用了HSI也不行 Translation: I need help. I used STM32H563VIT6 to configure a pin to output high and low levels. It works in debug mode, but not in normal operation (...

WYS666_0-1745228255395.png WYS666_1-1745228268624.png
WYS666 by Associate
  • 1116 Views
  • 2 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.