STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Voltage divider for ADC input?

OK, this is perhaps a fairly stupid question but I do not get it.I have an analogue voltage in range -5V..+5V and wantto measure it with the ADC of an STM32F446. The ADC-input works in range 0..3.3V.I have the feeling I can do that with a simple, res...

BSchm.6 by Associate III
  • 9697 Views
  • 5 replies
  • 0 kudos

OTA IN STM32U575 USING ESP32

IS ANY BODY HELP ME IN THE OTA OF THE STM32U575 USING THE ESP321. HOW TO SETUP THE SYSTEM BOOTLOADER TO RECEIVE THE FIRMWARE (.BIN FILE) VIA UART AND HOW TO SELECT WHICH UART TO USE FOR UPLOAD , THERE ARE MORE UART WHICH SUPPORT THE UART FLASHING HOW...

premkumar by Associate III
  • 3962 Views
  • 8 replies
  • 3 kudos

ISP Mode Programming in STM32

Respected Team, Following queries from my end,1. How to configure ISP mode programming in STM32L4? Which pins we can use to enable ISP mode programming in STM32 MCU?2. Is there possible to use UART based or any other interface based ISP mode programm...

ACM by Associate
  • 1413 Views
  • 1 replies
  • 0 kudos

Cortex M7 Hard Fault Handler - freeRTOS Aware

Hi All, We all know how hard it often is to track down the cause of hard faults, particularly random or intermittent ones when the debugger isn't connected and particularly when using freeRTOS in a complex system with many tasks, timers and queues.  ...

STM32H747I MDIO - can it goes until 32bit

I am using STM32H747-DISCO board for development, and I try to access for MDIOs connectivity of the STM32H747, I found a document describe about MDIO:STM32H7-Peripheral-Management data Input Output slave interface (MDIOS)From the document it describe...

Khey87 by Associate
  • 1267 Views
  • 2 replies
  • 0 kudos

Resolved! reset problem

hi, im using stm32g474vet6 mcu for power converter. when the supply is turned on initially first time, controller is behaving like hang or stuck somewhere. if i do a pushbutton reset, the mcu starts working fine. after that no issue. whenever im turn...

Resolved! STM32F030R8 PSPICE model

Hi, As I am doing a Pspice simulation, for which I am using STM32F030R8, I need the Pspice model of STM32F030R8. To use the GPIO Functionality to connect the MCU to the simulation circuit in LTspice or OrCAD Pspice.

nandhini by Associate
  • 1157 Views
  • 1 replies
  • 1 kudos

Resolved! 800KHz Frequency generation using STM32G070RBT6

I am trying to get 800KHz frequency with Timer 3 and timer clock is 64MHz and i am using below setting to initalize the timer, but its frequency is 666.66KHz. Pls provide a solution of this problem ASAP......   static void MX_TIM3_Init(void) { /...

Preetpal by Associate II
  • 1665 Views
  • 2 replies
  • 2 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.