STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Interfacing STM32F722VET6 With Quad Memories

Posted on June 13, 2018 at 10:35Hello,I want to interface 512Mbit or 1Gbit I  with  STM32F722VET6 with CubeMX . I have seen lots of option for interfacing  ..Which option I need to select for below memory chips in Quad SPI Mode , Bank (s) and Why ?....

0690X0000060LEGQA2.png

CAN STM32F303

I USED HAL_CAN_AddTxMessage FOR TRANSFER MESSSAGE BOUT I NEED KNOW WHEN THIS MESSAGE IS FINISH BEFOR START NEW MESSAGE

Resolved! Load program using Micro-B USB

Hello,I'm using STM32F030 series controller. currently we use JTAG connector to load a program into flash memory, using ST-LINK debugger externally.Now i want to load a program into flash memory using Micro-B USB in my device without using any extern...

SPraj.15 by Associate II
  • 2740 Views
  • 5 replies
  • 0 kudos

STM32F4: EXTI: Fails to capture rising edge interrupt sometimes

In out project we are making use of EXTI for interfacing a radio (RF) ASIC with STM32F411. Whenever, the radio has some data to be sent host it interrupts the host using the I/O line (drives the line high). This I/O line stays high till data is read ...

MSuhe by Associate III
  • 6039 Views
  • 15 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.