STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32 USART synchronous mode receive does not work

Hello,I am using a STM32L052K6U6 to communicate with an SPI slave using the UART1 synchronous mode (configured with CubeMX, using the LL library).This is part of the code that receives data:while(!LL_USART_IsActiveFlag_TXE(USART1));LL_USART_TransmitD...

Fr4nky by Associate II
  • 3507 Views
  • 5 replies
  • 0 kudos

mcu halt when a Contactor is turned on

i have a an stm32f417vgt6 mcu and its connected with ft800 through 30 cm SPI cable and the ft800 is driving a tft lcd .. the problem is when the mcu turn on or turn off the Contactor the mcu halt .. can you please help me how to detect the prob...

How to measure 3phase L-L 440 volt using STM32 ADC?

i want to build circuit that can measure AC voltage 0-600V AC using STM32 it there any sample circuit and example code of it..i have try some circuit ...1) 0-400v ac --> stepdown transformer --> 0-15v ac --> dc --> resistor divider --> adc pin MCU b...

Resolved! Connect STM32F4 with smart card ISO7816

Hi, everybody. My task is to connect STM32F4 discovery Board with Smart Card ISO7816. I don't use interface ST8024CDR only hooked paid directly by the scheme specified in the image:I tried to adapt the Cubex project to STM32F1xx-EVAL. ATR reception d...

0690X000008ANWeQAO.png

STM32F769 Discovery board capturing input on timer 3

I am trying to capture input from an external source. Using CubeMX as a guide, I configured timer 3 like this:/* TIM3 init function */ void MX_TIM3_Init(void) { // PC8 ------> TIM3_CH3 TIM_IC_InitTypeDef sConfigIC = {0}; GPIO_InitTypeDef GPIO_...

MPlan.7 by Associate III
  • 3185 Views
  • 7 replies
  • 0 kudos

Toggle Mode of Advanced Timers

Dear AllI am playing with TIM 1 to better understand its functionalities. My tests indicate that in the toggle mode (set through OCxM bits of CCMR): 1) The counter operates in the up-down mode, even if the CMS bits of CR1 are set to 00 (which is for ...

Amir1 by Associate II
  • 3450 Views
  • 5 replies
  • 0 kudos

How inaccurate is the RTC?

Hello! I wanted to know how inaccurate the RTC is when working with LSI or LSE.Reading from posts and data sheet of the MCU, I saw that LSI is much more imprecise than the LSE. I wanted to know if there was an equation that would allow me to estimate...

Emm1592 by Associate II
  • 3097 Views
  • 6 replies
  • 0 kudos

HSI clock and baudrate ?

Dear Members,I changed my clock from MSI to HSI but my SPI and UART baudrate becoming wrong,What do I miss here ?thanks

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.