2019-04-15 4:23 AM
Hello,
I'm using STM32F030 series controller. currently we use JTAG connector to load a program into flash memory, using ST-LINK debugger externally.
Now i want to load a program into flash memory using Micro-B USB in my device without using any external debugger.
Please suggest suitable circuit and possible solution.
Thank you
Solved! Go to Solution.
2019-04-15 7:01 AM
" on-board USB"
The board may have a usb port but the STM32F030C6 definitely not have.
So, between the computer and the device must have an interface like STlink or other SW adapter or a usb to serial adapter.
Btw, what kind of board you use?
2019-04-15 4:49 AM
Hi
STM32F030 can only be programmed by using USART on pins PA14/PA15 or PA9/PA10 or I2C on pins PB6/PB7 for STM32F030xC devices ,by invoking internal boot loader.
F070 devices have this capability to programmed from USB.
2019-04-15 4:52 AM
Does AN2606 suggest the ROM supports DFU mode? Check also build size of user based DFU code, and if that and your application code will fit in device.
2019-04-15 5:13 AM
Hello Vangelis,
Thanks for reply.
Can we load program using on-board USB in our device with STM32F030C6 if possible then please share a reference schematic.
Thank you
2019-04-15 7:01 AM
" on-board USB"
The board may have a usb port but the STM32F030C6 definitely not have.
So, between the computer and the device must have an interface like STlink or other SW adapter or a usb to serial adapter.
Btw, what kind of board you use?
2019-04-15 9:54 PM
Hello Vangelis,
Currently we are using micro-B USB for only battery charging purpose using Supply and ground pins of USB port.
As you said previously, flash memory is programmed using USART pin PA9/PA10.
So if i connect PA9/PA10 pin with the USB pin(D+ & D-), it is possible to load flash using this configuration, please suggest.
ST link will be needed external?
Thank you
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.